STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! What is _l in pin IO structure?

In the STM32L4P5xx datasheet, some pins' IO structure is labelled with _l (in combination with other letters). However, this letter is not explained in Table 14 nor anywhere else.Can this please be explained?Thanks,JW

waclawekjan_0-1768238977877.png

ADC and DMA on STM32F303

Hi, I run ADC1 with DMA on my STM32F303RE with 72MHz clock.  I take the number of samples flowing into the circular buffer per timeunit.  I calculate a sample freq. of 1.305 Megasamples per second Ms/s. When I look at the sampled known signal I calcu...

DetlefS by Senior
  • 573 Views
  • 2 replies
  • 0 kudos

Resolved! HAL_CAN_START returns 131072

Hi. I'm new to STM32, and I'm using STM32F103C8T6. I want to run Loopback mode to test CAN BUS without another board first. When I go to debug, I find it stuck at HAL_CAN_START. It returns error code 131072. Can you guys please help me find out the p...

Dang_VAA_0-1768189276590.png
Dang_VAA by Associate II
  • 1365 Views
  • 13 replies
  • 6 kudos

STM32 N6 Load and Run USART doesn't work

Hi,  I have been trying to deploy the 66GYMAI1 Camera on the STM32 N657X0Q Nucleo board with the Load and Run mode. However, there is a problem that I could not solve, which is that the project can not jump from FSBL to APPLI. Because I am trying to ...

HANITALY by Associate III
  • 742 Views
  • 1 replies
  • 0 kudos

TCPP03-M20 with STM32G0B1CBT6 failed to connect

Hello Expert, Could you please provide guidance on the issue below?  We are using the following setup:- MCU: STM32G0B1CCTx- Software: X-CUBE-TCPP 4.2.0 with USBPD Application 4.2.0 Dual Role- Board Part: TCPP0203 v1.2.3 We are developing a USB PD boa...

PaulMinh by Associate II
  • 1694 Views
  • 7 replies
  • 0 kudos

Resolved! stm32u5 CAN, How to cancel resend failed messages

hello:@mƎALLEm I'm currently working with the STM32U585 and ran into a problem abort CAN auto Retransmission.Context:There are three devices on the CAN bus: stm32u5, A and Bstm32u5 enable auto Retransmissionstm32u5 need to keep sending them messages,...

lll by Associate III
  • 251 Views
  • 1 replies
  • 0 kudos

Cross Reference

Pls cross  TI part number TMP75AIDGKR (Temperature Sensor With I2C and SMBus Interface) Previously there's a Cross Reference tool in ST website but it's gone. I use it regularly. I hope it can be reinstated. 

Hello World Error Program

I have a problem, where there's simply no error, but the output, is not showing on the screen. The system has detected the board, and all the correct steps are followed, even though, my hello world code is not been printed. I am using stm32cubeide ve...

Mohit79 by Associate
  • 556 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.