2026-01-12 1:47 AM
hello:
I'm currently working with the STM32U585 and ran into a problem abort CAN auto Retransmission.
I want to know:
Solved! Go to Solution.
2026-01-12 1:53 AM - edited 2026-01-12 2:08 AM
Hello,
The ACK is sent whatever it's recipient or not. The ACK has no relation with the ID but to the validity of a CAN frame.
So if A and B are recipients at least one of them will acknowledge the frame. So if A is offline, B will always acknowledge. Same thing, if B is offline A will acknowledge no matter the ID used.
2026-01-12 1:53 AM - edited 2026-01-12 2:08 AM
Hello,
The ACK is sent whatever it's recipient or not. The ACK has no relation with the ID but to the validity of a CAN frame.
So if A and B are recipients at least one of them will acknowledge the frame. So if A is offline, B will always acknowledge. Same thing, if B is offline A will acknowledge no matter the ID used.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.