STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! stm32 with 32 pins with FDCAN but without HSE?

HelloIm developing a CAN Bus node and with space constrains, so i ve looked in stm32 products and a qnf32 packages looked perfect for example stm32G0B1 has FDCAN. The problem...These QFN32 dont expose HSE pins. I just can use HSI with 16 MHz +- 1% wi...

ricardos by Associate II
  • 610 Views
  • 4 replies
  • 2 kudos

Using an STM32G484 OpAmp as a Shunt Sensor

 I'm developing a power bus manager where I monitor current and voltage drop across a shunt resistor. I chose the STM32G484 as the MCU because it has enough OpAmps and ADCs for my project.However, I have a question that might only be related to elect...

Resolved! STM32H56xx/STM32H57xx Stock and Lead Time

Hello,I would like to get information about the availability of the following devices:STM32H562IGK6 UFBGA 144 package (10 × 10 mm, 0.8 mm pitch)STM32H562IGT6Could you please clarify:Are these devices currently available in stock for production volume...

Resolved! Gravação mult

I would like to know how I can program 2 MCUs (stm32wb55cgu6) simultaneously.Currently, I am programming the FUS and BLE binaries (firmware developed by the company).We need to double production, but I can't program via DFU because an error always oc...

Resolved! Calibrating the STM32's real-time clock (RTC)

I have an STM32L011F4P6 with an RTC.  It is running at 3.3V and 16 MHz off the internal HSI RC clock.  The RTC is driven by a +/-20ppm 32.768 KHz crystal.  It is running at room temperature (23-25C).  After calibration, I am losing several seconds pe...

Resolved! STM32H723 SPI clock issue

In my project I've set the SPI clock to 125MHz; with a SPI prescaler value=4 all works good, when I set it to 2 the SPI stops working and ther is no clock signal.Any helps ? Thank youCarloV

carloV by Associate III
  • 1145 Views
  • 11 replies
  • 2 kudos

Resolved! HAL_UART_Init() assert with LPUART at high baudrate

I call HAL_UART_Init() with LPUART1 at 20Mbaud but when I activate assertion it fail at IS_UART_BAUDRATE().The IS_UART_BAUDRATE() is not correct for LPUART that can have a baudrate up to 53.3 Mbaud.Also for UART, the comparaison in IS_UART_BAUDRATE()...

nicolas by Senior II
  • 633 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.