2025-05-28 1:08 AM
Hi,
I have been trying to deploy the 66GYMAI1 Camera on the STM32 N657X0Q Nucleo board with the Load and Run mode.
However, there is a problem that I could not solve, which is that the project can not jump from FSBL to APPLI.
Because I am trying to jump from FSBL to APPLI to print something by USART, but it doesn't work.
I would be grateful if someone could check it.
2026-01-12 4:11 AM
Hi,
Which IDE environnement are you using ? Did you try to connect the debug with the software reset mode ?
Regards,
Simon
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.