2025-03-19 7:26 PM
Pls cross TI part number TMP75AIDGKR (Temperature Sensor With I2C and SMBus Interface)
Previously there's a Cross Reference tool in ST website but it's gone. I use it regularly. I hope it can be reinstated.
2025-03-19 10:56 PM
Welcome @eric_copelan, to the community!
The X-Reference search can still be accessed via the homepage. Depending on the browser, either via a drop-down on the left-hand side of the search field or directly in the search results. Just try it out on st.com!
Regards
/Peter
2025-11-17 8:42 AM
The cross-reference option is no gone... it was where we could load it in the search bar and it gives us all available crosses.
2025-11-17 3:05 PM
Welcome @tslater, to the community!
The Xref has not been removed, but is handled differently by different browsers:
Windows Edge
Chrome and, e.g. Brave browser
This is a little more specialised and only allows the above-mentioned alternative function:
I'm sorry that it's so hidden, but maybe this will help you.
Regards
/Peter
2025-12-23 5:38 AM
Hi Peter
I am also facing same issue, I have attached the image for your reference, previously X reference used to come by clicking on magnify glass option but now, I am not able to click on this option.
2026-01-11 11:25 PM
Hi Peter,
I am facing the same issue and cannot find the icon or the name of cross reference in the search bar.
Is this function fully removed from ST homepage?
Thanks.
2026-01-11 11:58 PM
As I mentioned above, the behaviour depends on the browser. Since you haven't provided any information other than the screenshot (e.g. operating system, browser, attempted solutions), it's difficult to formulate an answer.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.