STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Trouble with CAN Interrupt and Free RTOS

I am having issues with the use of HAL_CAN_RxFifo0MsgPendingCallback. I've set every configuration (filter, start, interrupt, notification, and priority), but the function doesn't seem to be called at any time.Most of the code is generated from the c...

SPI TransmitReceive wrong behavior

Hello ST expert.I'm trying to create SPI communication as shown in the CubeMX image.and the following code/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c ...

Paulo971_0-1716058239690.png Paulo971_1-1716058254335.png Paulo971_2-1716058418846.png
Paulo971 by Associate III
  • 4837 Views
  • 9 replies
  • 1 kudos

STM32G051G6U6 IWDG not refreshing

Hi,I am facing an issue with IWDG in  STM32G051G6U6.HAL_IWDG_Refresh(&hiwdg);  not refreshing IWDG and  the core resets after IWDG overflow time.IWDG overflow is set at 13Sec (varying wrt prescaler) and I am refreshing it at every 1 sec.Counter presc...

Resolved! Simple UART problem STM32H753

Hi,I'm relatively new to the STM32 world and I'm becoming frustrated that I can't make a simple UART work. No DMA, no interrupts just trying to send bytes out of the UART and then receive them. Here is my setup code:      void UART7_Init(void) { GP...

GlennH by Associate III
  • 6646 Views
  • 12 replies
  • 5 kudos

SPI lower harmonics problem with XPT2046 touch sensor

I had EMI problems interfacing with my 4.0" ILI9488 v1.1 display over SPI. Having a long cable (about 30cm) display and touch works when powered using ST-Link V2, but when i powered it using a generic 24V PSU, the display and touch is not working all...

Selecting RTC Internal wakeup line

Hi everyone!I have an u585 related question:Can I configure RTC internal wakeup line other than PWR_WAKEUP_PIN7_HIGH_3 ?In all u5xx examples used this line, but We have an external wakeup source on  PB.15.I can't change it in CubeMX and I can't find ...

ccuebler by Associate III
  • 3104 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.