STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32G474 default option bytes configuration

Hello,I've another observation, may be something wrong in board.host controller is sTM32H573 which will update firmware of slave controllers interfaced on SPI one is sTM32G071 and is STM32G474, I'm using nucleo-g474re boardfor sTM32g474 controller sy...

0693W000006FmJtQAK.png 0693W000006FmKNQA0.png 0693W000006FmKhQAK.jpg
AShel.1 by Associate III
  • 5816 Views
  • 3 replies
  • 2 kudos

Resolved! STM32C011F6U6TR Boot Mode Selection Problem

Hello, I will use STM32C011F6U6TR in a project.Since I need to program with USART, I think I need to use the "boot from system memory" mode in BOOT mode, am I right?As written on the datasheet, there are 3 modes. When switching between these modes on...

How to trigger input capture

Hello All,I want to trigger an input capture when another timer overflows. I have both timers set up, but I am missing on how to make the overflow event trigger the input capture of the other timer. The reference manual has been a good help, but I ca...

Banana123 by Associate II
  • 4230 Views
  • 6 replies
  • 4 kudos

TSC peripheral - Linear Slider

Hello,I have a board with a interlaced 4 segment capacitive slider, not half-ended, connected to channels G2-IO2, G3-IO2, G4-I02 and G5-IO2, so in the same bank but different groups, as it should be I suppose. Can anyone please tell me what comfigura...

Resolved! stm32h747i-DISCO display issues

I recently bought an stm32h747i-DISCO and tried to run 2 example projects the "JPEG_DecodingFromFLASH_DMA" and the "JPEG_MJPEG_VideoDecoding". Both of them run correctly on M7 processor, but it seems the display has an hardware problem because it tur...

AFato.3 by Associate II
  • 3751 Views
  • 3 replies
  • 1 kudos

Resolved! Is it ok to connect VDDIO2 Pin to VDD?

Hi,I am using STM32L071C8T6 which has a VDDIO2 power pin. I don't see any information on this pin in the STM32L0xx hardware dev reference. My application doesn't require a separate level or source for any GPIO's, so can I connect VDDIO2 directly to V...

icecats_0-1716374212586.png
icecats by Associate II
  • 1364 Views
  • 1 replies
  • 0 kudos

How to make a external NAND flash program algorithm?

Hi all,I am trying to program some data to an external NAND flash chip(connected by FMC) by STM32F429BI with MDK IDE.According to the ARM document, I make a project(download it in the attachment) to generate the FLM file.(Before compiler the project,...

Junde_0-1716370895046.png
Junde by Senior III
  • 1699 Views
  • 0 replies
  • 0 kudos

Resolved! STM32F303VET - issue in transmitting CAN messages

I am having an issue in transmitting CAN messages, my situation is the following:There is an interrupt function for RX messages from CAN1, when a message is received, it sets a flag. The baud rate of the RX message is 10ms and they are being sent ove...

GComes by Associate III
  • 4005 Views
  • 7 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.