STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Timer Commutation Event Callback not firing STM32F429

EDIT* for those seeking a solution, JW in the replies below pointed out that the DIER register for TIM1 never enabled the interrupt bit for the commutation event and the mistake was that I used HAL_TIMEx_ConfigCommutEvent(&htim1, TIM_TS_NONE, TIM_COM...

tim1_conf.png tim1_conf2.png tim1_conf3.png
DNG_Gabbi by Associate III
  • 5304 Views
  • 8 replies
  • 2 kudos

Resolved! I-CUBE-USBD-Composite

Hey, just wondering if you could help with the following? We are using a package called I-CUBE-USBD-Composite for combining two USB classes. We use CDC class for serial communication and HID class for MIDI. We change the descriptor for custom HID cla...

Resolved! HAL_I2C_Mem_Read, no NAK send out

Hi There,While reading the data from I2C, I see that the master is missing to send NACK.Some fixed was done in https://github.com/STMicroelectronics/STM32CubeF4/issues/139 but those fixes are there in the code. But still sometime i see that NACK not ...

Screenshot 2024-05-30 140540.png

STM32 CANBus bootloader - verification errors

Heads up about a problem we discovered, and I think solved.  We're using the built-in STM32L452 bootloader per AN3154 to do in-system firmware updates over CAN bus from an Android host.  We started with the can-prog Python utility (https://github.com...

Brian Rau by Associate III
  • 1649 Views
  • 1 replies
  • 1 kudos

Resolved! STM32G0B1VET6 100-LQFP Reference Design

Hi, I am MURALI SELVAM from DNCL Technologies, I need reference schematic for STM32G0B1VET6 MCU, If anyone have reference schematic. Kindly provide me. Thank you.

murali by Associate III
  • 2874 Views
  • 5 replies
  • 3 kudos

STM32U5 board can't connect to cubeprogrammer

Hello,I had two STM32 boards connected to the PC, and I ran the regression.sh program from SBSFU to configure one of them. However, the second board, which also had the SBSFU application installed, was configured as well. Now, the second board cannot...

Istillaga_0-1717143331135.png Istillaga_1-1717143443704.png

Resolved! What can cause UART overrun error while using DMA for reception?

Hello,I am implementing a Modbus Master on a STM32F722. First, transmissions and receptions were managed through Rx/Tx interrupts. But as I got a lot of overrrun errors while getting my slave's responses, I decided to transfer received packet through...

ABous.3 by Associate III
  • 6991 Views
  • 7 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.