STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F466VET7 Program and Debug

Hello everyone,  I am designing a PCB and I need a ST-Link connection for debug and programming. This is my first time in this kinda stuff so I need some help.Which one should I have to use for debug and programming?As I understand Serial Wire is for...

testbenchmark_0-1717243575981.png testbenchmark_1-1717243812828.png

HAL UART DMA functions

Hi,I need a DMA setup for 4 separate UARTs in an STM32G473 controller. The idea is to always be able to receive data through rxDMA, and only invoke txDMA when sending data. The data that I receive changes in size, is between 20 and 300 bytes, starts ...

sde c.1 by Senior II
  • 2456 Views
  • 1 replies
  • 2 kudos

With a strange error display when I use input capture

Hello!  My project is almost finished, but I had a little problem. On the dashboard, I can optionally read the speed and coolanz water temperature from the can bus or with sensors (vr sensor, ntc). In the case of the can bus, the display works proper...

My code stuck at HAL_InitTick() at the beginning of the code

I am programming my custom board with STM32G491CEU6 and STM32CubeMX 6.5.0.The code is generated with STM32Cube_FW_G4 v1.5.1 firmware.Steps to reproduce:Select 'access to MCU selector' after opening STM32CubeMX.Select STM32G491CEU6 and create the proj...

KWang.9 by Associate
  • 8489 Views
  • 8 replies
  • 2 kudos

Resolved! Ethernet - without RTOS or CubeMX - STM32H7

Hello,I am hoping i can be pointed in the right direction.I would like to create, using an STM32H7, a device that has an ethernet port. The idea is simply to go to various sites and scrape info for processing later on. I guess this will require TCP/I...

CEagl.1 by Associate III
  • 3910 Views
  • 2 replies
  • 3 kudos

Read NMEA Data via UART STM32

HelloI am currently working on a microcontroller project I am building a GPS tachometer which transfers the NMEA data of the GNSS 4 Click Module from Mikroe via UART to my STM32L052K6T6 and outputs it to a displayI have so far UART initialized with t...

MSchmutz by Associate II
  • 8620 Views
  • 7 replies
  • 3 kudos

STEVAL-MKBOXPRO firmware upgrade, Unicleo GUI and IDE

Hi, [1] I have this board STEVAL-MKBOXPRO. on my PC, I have installed all ST software [IDE, CubeMx, Uni-cleo GUI, Unico GUI, AlgoBuilder Suite].[2] I have connected this board via USB-typeC to PC. Questions[Q1] Uni-Cleo GUI does detect the mkboxpro a...

vlsireddy_0-1717017952186.png
vlsireddy by Associate II
  • 1905 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.