2026-01-22 7:56 AM - edited 2026-01-22 7:56 AM
During RTC init when RTC_EnterInitMode is called a unit sets the INIT bit of the RTC_ISR register in the HAL but when it waits for the bit set to respond it times out with the bit never being set. I have run this same firmware on hundreds of other units with no issue. If the INITF does not set is it likely due to an internal issue of the microcontroller?
2026-01-22 8:11 AM - edited 2026-01-22 8:13 AM
RTC clock must be set and running. Check RCC_BDCR content and if you've selected LSE as RTC clock, make sure it's running.
Also, make sure the backup domain access is enabled in PWR_CR.DBP (again read it out and check - a quite common error is forgetting to enable PWR clock in RCC) and the proper write-disable sequence has been performed with RTC_WPR.
JW
2026-01-22 8:27 AM
Sure i can check those registers. I assumed that if the RCC LSE init succeeded that it was running but i can go back and double check. With the backup domain access is there anything unique about that that one unit out of 300 is exhibiting this? I can definitely put it in but would have expected this to be a more recurring issue. I could believe that the LSE not being correct could be the issue in this case though.
Thanks for the feedback
2026-01-22 8:31 AM
> I assumed that if the RCC LSE init succeeded that it was running
How do you check that that init succeeded?
> With the backup domain access is there anything unique about that that one unit out of 300 is exhibiting this?
I have written wilder bugs than just that... ;)
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.