STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! 'U5 SBus-via-DCACHE1 connectivity

Is this connection real?I don't think so. DCACHE implementation subchapter says:The DCACHE1 is placed on Cortex®-M33 S-AHB bus, and caches only the external RAMmemory region (OCTOSPI, HSPI, and FMC), in the address range [0x6000 0000:0xAFFFFFFF] of t...

waclawekjan_0-1768924913136.png

STM32U5 Traceclock

HelloI trying to figure out what the maximum frequency is for the TRACECLK  stm32u5A9.I found this post for the stm32h5https://community.st.com/t5/stm32-mcus-products/traceclk-freq-in-stm32h5/td-p/604127does the same apply for stm32u5 were can i in t...

Sebastian33_0-1768552686257.png

Resolved! Can we use RTC timestamp with standby?

We have a STM32H725 and would like to use the RTC timestamp when entering/exiting standby but from what I understand from the reference manual this is not possible? I did run a quick test and the event doesn't seem to fire even though it works as exp...

obj87 by Associate II
  • 633 Views
  • 6 replies
  • 1 kudos

Resolved! Software triggered One Pulse Mode – more than once

Hi,I'm trying to generate a pulse of a fixed length when my application triggers it, on one of two timer outputs, depending on a boolean value. My problem is that it works only once. The first time I start the timer, I get a nice pulse, but the subse...

EThom.3 by Senior III
  • 411 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.