2026-01-20 2:45 PM
On the STM32N6, half the ram is attached to this NPU RAM on it's own bus. Are there any downsides to using this ram for non neural net applications.
Use case
I would like to use the NPU ram for just frame buffers.
From what i can tell the memory is continues so i could put a memory buffer across potentially 2 different AXISRam sections.
Just asking if i would be able to use DMA operations with the DMA2d or the GPU2.5D engine. Or if i could DMA peripheral like SPI or LTDC from these buffers
Related post
Solved! Go to Solution.
2026-01-26 1:29 PM
You'll need to turn those RAM regions on before you can read/write to them, but other than that, they're normal SRAM! Just gotta expand the Linker script to include it in RAM or make a new region.
2026-01-26 1:29 PM
You'll need to turn those RAM regions on before you can read/write to them, but other than that, they're normal SRAM! Just gotta expand the Linker script to include it in RAM or make a new region.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.