STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 in Stop2 mode (Debug vs Release)

Good morning,I have an application based on the STM32L475 device that is running in many devices since many years ago. We have observed that, sometimes, some of the devices are resetted --> Here you have the main specs of my device:- Device is workin...

Resolved! USBPD CC orientation STM32G071RB

Hi, I am troubleshooting a custom board using USBPD as sink. It only negotiates a PDO on one orientation of the USBC connector.Checked with an oscilloscope and I see waveform going to CC1 on the orientation that works , naturally, and changing orient...

josemdq by Associate II
  • 5330 Views
  • 10 replies
  • 0 kudos

STM32F407 CDC Host - IN transaction always returns NAK

I've setup an STM32F407 as a CDC Host on the HS peripheral with Full Speed (FS) comms, but the IN transaction always returns a NAK and no Device data is received on the Bulk Data pipe. I used the USB Host example from ST.com (userfunction that only t...

0693W000004KK8VQAW.jpg
Paulus by Associate II
  • 7242 Views
  • 6 replies
  • 0 kudos

Resolved! FDCAN interrupt not working

Hello,  I am trying to make FDCAN work but I am not receiving any messages. The TX is working fine but when trying to receive messages the interrupt is not triggered. I am using STM32H7 series with freertos. I have set the filter, started FDCAN, enab...

PPopo.1 by Senior
  • 4477 Views
  • 5 replies
  • 2 kudos

mmc deinit problem

Hi, We are working on a low power application which uses an emmc memory. Now we have problem when Deinit mmc driver. When mmc is disabled we have a base consumption of XXuA (stop 2 power mode) but when it is needed mmc must be enabled (using Init fun...

cgamu by Associate
  • 1809 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F446 Tempreature Sensor, ADC

I am trying to read ADC value of internal tempreature sensor of my STM32F446 board. The data sheet says that the temp sensor is connected to ADC1_IN18 (page no. 37/198), but there is no such pin in STM32F446xx pin and ball descriptions. Can someone p...

Resolved! ADC1, ADC2 dual mode with differential input

ADC1 and ADC2 run in interleaved dual mode using DMA. Resolution for both ADCs is set to 8-bit. ADC1 is sampling CH1 and CH2 in differential mode. The results that I get from DMA are a bit strange: If my positive input is ~1.65V, if my negative input...

graph_adc.png table.png
CyberNerd by Associate III
  • 1496 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.