STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! CMOS- and TTL-compliant

Hi,Master:platform: STM32G070CBQuesion:       Regarding CMOS - and TTL compliant, the manual provides the above diagram. How does it achieve compatibility? When Vin>min (07 x VDDIO, 2), is it considered that the input is at a high level? When Vin<min...

q.jpg
Lyu.1 by Senior
  • 3304 Views
  • 5 replies
  • 0 kudos

Resolved! Bootloader initialization concern with STM32G0B0R

Hi, Please advise . I've been designing with the STM32G0B0R at my company. I have some ports connected to a ULN2003A driver input and ouputs to a relay's negative return, since the relay is conneted to 12V . specifically PC10, PC11. PC12,PC13. the UL...

GZ1 by Associate
  • 1684 Views
  • 1 replies
  • 0 kudos

STM32H563 read from flash bug

Hi, I have an IAP project which have image A and image B. Image A is on flash bank1 and image B is on flash bank 2. When I run image A and upgrade image B, I will trigger the bug when doing soft CRC. The system is running on freertos.My soft crc code...

stc.png Capture.PNG
Ehow by Associate II
  • 1592 Views
  • 1 replies
  • 0 kudos

STM32 MCU CAN clock register default value

Hello folks,Anyone knows the default CAN clock frequency on STM32H753 MCU when powered on, assuming the CAN bit timing register (CAN_BTR) was not set by FW during the initialization?If this value would be a random, could it be changed depending on re...

fourhes by Associate II
  • 1918 Views
  • 6 replies
  • 0 kudos

FFT spectral resolution not enough

Hello comunity, I am using the CMSIS DSP library in order to perform FFT to 1412 sample set with a sampling freq of 16.83Khz. I am trying different approaches to find the 16th harmonic after the fft, but i get an inaccurate value. for example, Zero-p...

arm-none-eabi-size STM32CubeIDE Version: 1.16.0

I USE STM32CubeIDE Version: 1.16.0 when build the project massage arm-none-eabi-size and the hex elf or bin files after download to stm32f107vct6 no actions nothing also i use cubemx last ver for generation code thanks

EG by Associate II
  • 1990 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 CPU clock vs GPIO clock

Hiwhat is the relationship between the speed of the CPU and the GPIO response. for example, I have a CPU clock of 72MHz and a GPIO clock of 36MHz and I set the pull-up when is this pull-up visible to the CPU because e.g. I would like to read the port...

sholojda by Associate III
  • 2490 Views
  • 4 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.