STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32h753bit6 HSI clock at startup

tying to find what frequency the hsi is at startup  and normally i search the datasheet for clocks and startup but this returns nothing in the datasheet for the stm32h753bi mcu only thing i see is that it has 4 clocks and it says the hsi is 64mhz is ...

Resolved! Debugging application from external flash

Hi All,I have interfaced  Winbond W25Q128 external flash and IS42S32400F-7TL external RAM to STM32H750IBK micro on my custom board. I have found an external loader file (stldr) for my pin configuration from a community member.I can program, read and ...

Kutlu by Associate II
  • 11818 Views
  • 8 replies
  • 7 kudos

Resolved! Parallel RGB interface in STM32-F411RE

For my project, I need to use a parallel RGB interface (8 bits) to control a display using Nucleo-F411RE. The PCLK for the RGB interface is required to be a minimum of 1MHz.However, the STM32-F411RE does not have any LTDC peripherals. So I implemente...

Soad by Associate II
  • 1568 Views
  • 1 replies
  • 1 kudos

USART interrupt handling in Rust

Hi, I'm new to embedded (as in one week old) and am trying to build a small system to do a few things for an optical product we're building: mainly temp measurement (Omega SA1-RTD with MAX31865) and LED management for optical lasers. Currently I have...

sekhar by Associate II
  • 8355 Views
  • 14 replies
  • 6 kudos

w25q128 external flash with stm32l412

Hi,I am using stm32l412 controller with an external flash w25q128 in quadspi mode. I am able to read and write on to the flash memory. but I am unable to use it as an external loader. I referred many tutorials, I edited the linker script to add a sec...

hash002 by Associate II
  • 2023 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 MCU die

Hi all,Can anyone confirm if these two type of STM32 MCU, STM32H753BIT6 and STM32H753VIH6 use the same die although they have different packages? Best fourhes

fourhes by Associate II
  • 2668 Views
  • 4 replies
  • 5 kudos

Resolved! Alternative Functions and Additional Functions

STM32L072 has USB as Additional Functions instead of an Alternative FunctionThough in one of my Earlier Post It was briefly explained, It felt to have a Dedicated Post in General Thereby this Post to Better Understand the Difference and Way of Workin...

Pavan_LohiaGroup_0-1724038285746.png

Resolved! STM32F411CEUx USB Serial Port Issue

I am having trouble configure the USB-C port for serial output. The board I got is a "BlackPill" and I have went to try some example code for USART2 and USART6, however, upon a reset, I still do not have a COM port appear. Any advice?

dlaroche by Associate II
  • 1437 Views
  • 1 replies
  • 1 kudos

The MCU requires NRST to be toggled after power on

Hi all, I have a problem with a new version of an existing PCB using the STM32F334C8T6 microcontroller.Known working code is loaded onto the new PCB, power is applied and the MCU starts up the clock and then seems to sit idle. If the NRST pin is then...

PXL_20230922_103355658.jpg PXL_20230927_100625674.jpg
RobertK by Associate III
  • 19681 Views
  • 38 replies
  • 8 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.