STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F105RCT6

in the process of or at least i want to backup the mcu data and transfer it over to another mcu,  i can connect and see the mcu with my pe cyclone fx but when i read and dump the data i get a empty file 768kb.     S31508000000000000000000000000000000...

brt2015 by Associate II
  • 9048 Views
  • 21 replies
  • 0 kudos

SDMMC impssible to get working

Hello,I'm using a custom board and have gone through 3 iterations one with stm made EMI filter for SD, one with F2 chip with SDIO and now I'm using stm32l496zg with 4.7k pullups on D0-D3 and CMD lines. When running the completely unchanged code gener...

Resolved! Rename project and also directory in STM32CubeIDE

When renaming a project in the project tree view it seems one can rename the project itself but not the directory it initially had been created in.I have a project "myfirst1", renamed it to "myfirst" with all references. In the treeview one can see t...

chriskuku by Senior III
  • 13678 Views
  • 10 replies
  • 3 kudos

Resolved! Max toggle rate using timers on stm32h503rb6

I am trying to toggle PB6 gpio at 10MHz on the nucleo board. I am trying to use timers to do this. Using LL library with full optimization and 250MHz system clock rate. I was able to get 3.5MHz ish. With timer 1 prescaler and divider being 0. Please ...

Resolved! PCB Customization

Good Afternoon Sir/Mam, We are Engineering Students. We have a PCB Design and I want to get it manufactured. We want it's single piece for our Prototype Development and Testing, once our Prototype completes the requirement criteria, we will order it ...

Ankur_1 by Associate II
  • 1935 Views
  • 3 replies
  • 0 kudos

Resolved! Graph

Hi, any provision to plot array data in real-time during debug using F439 Nucleo?Please guide

GauravK by Senior
  • 941 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.