STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32U575ZITxQ Port G GPIO Issue

I have just started evaluating the STM32U575ZIT6QU for a project that my company is working on.While attempting to evaluate the I2C pins for I2C1 on pings PG13 & PG14, I noticed that the pins would not work correctly and would stay low, even with int...

Resolved! RTC Drift

Hi,I have a custom board by STM32H743 and have some problems by RTC. I've used LSE with a 32.768 KHz external crystal. I have 2 or 3 seconds more in each minute. There is no reset within 3 minute and I see about 15 second more.I've used 6.8 pF for CL...

MHaji.1 by Senior
  • 1486 Views
  • 1 replies
  • 0 kudos

Resolved! Problem with selecting HSE as system clock

Hi Every one.When i am trying to write CS bit of RCC_CFGR register of STM32G491RE MCU to select HSE as a system clock (i.e 10) it changes to 11 (01 is default so i guess i am not able to clear these bits before assigning new value). Can anyone tell m...

srbhktyr by Associate II
  • 1529 Views
  • 2 replies
  • 2 kudos

Resolved! systick handler keep pending on stm32h7 board.

I made a project with stm32h7 board, and use pemicro multlink to debug it under keil. I found it keep in systick handler pending but no active.I checked systick module register as:the counter is changed.and then I checked SCB releate registers asand ...

shengyang_0-1725578415036.png shengyang_1-1725578563853.png shengyang_2-1725578660534.png shengyang_3-1725578726103.png

Read 3 analog signals; 5 - 20 kHz sampling rate

Hello,I have two core boards:1st: Nucleo-64 with STM32L476RGT6U 64 pins, 1Mb of flash memory and 128 Kbytes of SRAM.2nd: Nucleo-144 with STM32F429ZIT6U with 144 pins, 2Mb of flash memory and 256+4 Kbytes of SRAM.I have a little experience only with P...

Resolved! FSMC - TFT - STM32F7 Series

hi,I am trying to connect ili9341  - STM32F722ZE FSMC- TFT but i couldn't succeed .ili9342 16bit - is working in direct GPIO 16 bit data PORT drive with STM32F722ZE not in FSMC-TFT . Looks most of the ili9341 working with FMC-TFT STM32F4 Series   aro...

MMARI.1 by Senior II
  • 1184 Views
  • 1 replies
  • 0 kudos

Systick interrupt handler stopped being called

Hello STM32G0B1 For some obscure reason, sometimes the systick handler function is not called anymore.I mean, it works for some time then it does not work anymore. It looks like it is more likely to happen when I'm debugging but I have no factual inf...

JulienD_0-1723030099147.png
JulienD by Senior
  • 7140 Views
  • 13 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.