2022-11-12 12:28 AM
When renaming a project in the project tree view it seems one can rename the project itself but not the directory it initially had been created in.
I have a project "myfirst1", renamed it to "myfirst" with all references. In the treeview one can see that it has been renamed, but there is still marked like:
myfirst (in myfirst1)
Trying to rename myfirst1 to myfirst behind the curtain leads to things getting messed up.
How can I achieve this cleanly, so that "in myfirst1" disappears and the project is located in directory "first" in the filesystem?
Solved! Go to Solution.
2022-11-13 2:41 AM
I dont use it on MAC, but point 4 you can do too right click mouse on project explorer,
choice Import - General - Existing ...
2022-11-12 2:46 AM
2022-11-13 1:59 AM
Only works partially. It's macOS. Besides from making dot files visible in Finder (which I got working), double clicking does fire Xcode instead of STM2CubeIDE. How do I import a .project from within STM32CubeIDE?
2022-11-13 2:41 AM
I dont use it on MAC, but point 4 you can do too right click mouse on project explorer,
choice Import - General - Existing ...
2022-11-13 3:09 AM
OK, thanks. Tweaked it otherwise now by editing all files accordingly. Only one Debug configuration got lost but maybe I can get it from a backup or re-create a new one. Next time I'll follow the above steps.
2022-11-16 12:07 AM
5. Clean Project
6. Build Project
2022-11-18 7:59 AM
I'm still trying to recover from the mess I produced when trying to rename the project. At the moment I cannot see the projects .ioc file in the tree. But there actually is the file. I copied one instance of it from a tar file I previously produced from the project tree. But CubeIDE doesn't recognize the .ioc.
2022-11-18 8:07 AM
ioc + mx renaming is other story, because this i never rename projects only rename folder
and see it as (in folder) = ok
ofcourse cant have more as one this project in one workspace.
2022-11-18 9:28 AM
@MM..1 Sorry, but I don't understand what you are saying, in other words I cannot get any information out of it that helps me to solve my problem.
EDIT: solved it. CLEAN project made the file visble again in the treeview.
2022-11-18 9:50 AM
Sorry i only report my solution. But for help recovery , have you any backup?
ioc original is helpfull.
Maybe this steps helps:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.