STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Flash writing is not working

Hello, Flash writing is not working.When i update firmware, then Writing is working well only one time.But after this time, result is fail in HAL_FLASH_PROGRAM()  MCU : STM32F446RCT7  Thanks.

TaronKim_0-1730701297775.png
TaronKim by Associate II
  • 2286 Views
  • 4 replies
  • 0 kudos

Resolved! External crystal required for bootloader?

HiThere's a not-too-well worded paragraph from AN2606 on page 33:For STM32 devices embedding bootloader using the DFU/CAN interface in which theexternal clock source (HSE) is required for DFU/CAN operations, the detection of the HSEvalue is done dyna...

GMeta.1 by Associate III
  • 4206 Views
  • 7 replies
  • 1 kudos

STM32F3 Series Oversampling

Hi.  We use the STM32F3 series for a number of products.  We were hoping to implement oversampling for the two ADC's based upon the Application Note AN5537, which indicated in Table 1 that the STM32F3 series has the oversampling engine on chip.  Howe...

BVA by Associate II
  • 2108 Views
  • 3 replies
  • 0 kudos

HAL_FLASHEx_Erase error

I'm trying to store a simple runtime setting in flash memory of a stm32f103 with 64kb of flash.In my testing I'm targeting the second to last page at 63 with address 0x0800FFE0I can write fine to empty pages using HAL_FLASH_Program() but any call to ...

pulsar by Associate II
  • 2468 Views
  • 4 replies
  • 0 kudos

Resolved! Building CT-VPD dongle with ST products

Hi all.Are there any guides on building the charge-through VPD device with the ST product? An illustration from the standard: The goal is to maintain the smartphone's supply from the external PD charger while maintaining the connection with a USB 2.0...

VasylV_2-1727761563566.png
VasylV by Associate
  • 2194 Views
  • 3 replies
  • 1 kudos

Resolved! STM32F105xx SPI2 Does Not Drive NSS Pin High when Idle

I'm using the ST Cube environment (IDE + MX) to configure the SPI2 peripheral in Full-Duplex Master mode on a STM32F105VBHX chip.It seems like the peripheral is not driving the NSS (chip select) pin (PB12).  When the pin is selected for SPI2_NSS and ...

Brian H by Senior
  • 4862 Views
  • 8 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.