STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! fdcan on Riverdi STM32H7 Embedded Display 7"

Hello,I've started to develop with the Riverdi STM32 Embedded Display and I'm trying to use the CAN BUS to display data, but unfortunately I can't. I'm not receiving any data. The CAN on the board is a FDCAN and I've set it to classic, because that's...

Continuous DMA from memory to SPI

We need to continuously DMA a single 16-bit word to the SPI transmitter. (Neither the memory address nor the peripheral address would increment.) Can this be done without intervention? I.e. do we have to use a DMA Complete interrupt to set a flag and...

SoCalJim by Associate III
  • 9011 Views
  • 16 replies
  • 1 kudos

Resolved! BOOTING STM32F469

@STOne-32 , @Peter BENSCH, @Tesla DeLorean HI! I have my wiring below and I wonder what is wrong with it. Hope someone can give me some help!! my BOOT0 -> LOW, PDR_ON -> HIGH, BYPASS_REG -> LOW. And I have the following connections to the ST LINK:NRS...

kicad_cropped.jpg kicad_1.jpg

Using I2C Communication Protocol with LCD

STM32F407G DISC-1   STMCubeIDEGreetings, I am trying to send data to LCD screen by using I2C Communication Protocol. I succeed in doing it by using HAL library. Also, my current work does work in debug mode.However, I could not make it work by runnin...

Resolved! STM32H7A3ZI-Q getting random values from ADC

Hello, I'm currently trying to develop a bare-metal ADC driver for my Nucleo STM32H7A3ZI-Q Board. I have done all the necessary steps in order to setup the ADC, however I still get random values from the data register, even though I have my PF11 (or ...

ikok07 by Associate
  • 1682 Views
  • 2 replies
  • 0 kudos

STM32N6x7 - Wireless Time Synchronization

Hi,My team would like to design an array of indoor embedded boards using the STM32N6x7 processor (for AI support). We need these boards to synchronize their time / clock wirelessly.Does STMicroelectronics have any existing products or plans for a sol...

MikeE by Associate
  • 1589 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.