STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32L051C8T6 not executing the code properly

I developed a basic code in STM32CubeIDE to test an STM32L051C8T6 microcontroller, aiming to toggle the state of two LEDs connected to the custom-designed board for this chip. However, during debugging, an issue occurs with the execution flow.After i...

Resolved! STM32U575 Temperature Sensor ADC4 calculation

Hi,Currently I am trying to measure MCU junction temperature on the STM32U575 via ADC4 TEMPSENSOR channel (CH13). Upon reading the datasheet and reference manual of the chip, I have some questions regarding this implementation.According to both the d...

phuocly_0-1736237001109.png phuocly_1-1736237082283.png
phuocly by Associate II
  • 3128 Views
  • 6 replies
  • 3 kudos

Resolved! STM32H573 XSPI strange behavior

Dear Forum Members,I'm developing a hardware with a small LCD screen which is using a QSPI interface. I succeeded with an STM32H723 with its OCTOSPI interface through DMA, and I got good results, but I encountered memory mapping problems with the com...

PThiering by Associate II
  • 1484 Views
  • 1 replies
  • 0 kudos

Help with HPDMA + ADC on STM32H7S3L8

I've been trying to get DMA to work on the STM32H7S3L8 with bare metal code. As far as I can tell, I have everything set up correctly(?). I get no DMA error flags. The DMA complete flag is never set and the target buffer remains empty.I have enabled ...

chintal_1-1736421059030.png chintal_0-1736419377359.png
chintal by Associate II
  • 1618 Views
  • 2 replies
  • 0 kudos

interference of ADC channels in STM32F103RCT6

HI everybody,I purchased this batch of MCUS and found a difference in performance compared to my previous batch 19+,Unusual: The upper left corner is the standard source output setting, and the right side is the data detected by the product. Focus on...

jason110_0-1736410161380.jpeg jason110_1-1736410172201.jpeg jason110_2-1736410182557.jpeg jason110_3-1736410239227.jpeg
jason110 by Associate
  • 1353 Views
  • 1 replies
  • 0 kudos

VCom port, emptying buffer.

Hello! Not sure it's the right place to post. I have a custom board based on STM32F767. I'm using USB with VCOM port to communicate by UART. Basically it works (I mean, I can receive bytes from a terminal (I'm working on Ubuntu with STM32CubeIDE v. 1...

PG.1 by Associate III
  • 1815 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.