STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem with ST SPI on STM32L475.

Hello, I am using STM32L475 board and trying to communicate with VNF1048F by SPI. The communication protocol which is used is defined as ST-SPI. On STM32 I can configure at maximum 16 bit communication but the device (VNF1048F) requires 32-bit frame...

_legacyfs_online_stmicro_images_0693W00000bhx83QAA.png _legacyfs_online_stmicro_images_0693W00000bhx1KQAQ.png _legacyfs_online_stmicro_images_0693W00000bhx9VQAQ.png
KPerg.1 by Associate II
  • 2503 Views
  • 4 replies
  • 0 kudos

STM32H7 SAI TDM output

Hello,I am considering the STM32H7 for a new project I'm working on.I'd like to configure the MCU to output 10 audio channels at 96khz using TDM, all synchronized. Some variants of the STM32H7 come with up to 4x SAI peripherals and support TDM.I'd li...

messna by Associate
  • 1106 Views
  • 0 replies
  • 0 kudos

STM32 internal oscillator drift over time

I designed a board using a STM32L031F6P6 about 4 years ago,  (April 2021).   The design has been using the internal oscillator running at 16Mhz perfectly for years.   Then this past summer all of a sudden the RS232 Uart stopped receiving data until I...

npreiser by Associate II
  • 3707 Views
  • 7 replies
  • 2 kudos

SSI and Circular DMA

Hello!I am writing a driver for the mt6701ct rotary magnetic encoder, using cubeIDE and an stm32f405 MCU. This sensor communicates via SSI, which is to say that it's read-only (MISO-only; there is no physical connection to MOSI). Using a simple polli...

Screenshot 2025-01-14 at 8.17.05 PM.png Screenshot 2025-01-14 at 8.21.15 PM.png Screenshot 2025-01-14 at 8.15.52 PM.png
sb_st by Senior II
  • 3205 Views
  • 6 replies
  • 1 kudos

Resolved! PWM no signal on TIM2 Channel1 and TIM3 Channel 1

I want to generate 6 PWMs using channel 1 of timers 1,8,2,3,4,5. All of them are set the same way except ARR, PSC and CCR1 registers. However, it turned out that timers 2 and 3 don't have PWM signal on their pins. The content of registers for those t...

Dan_Ko by Associate II
  • 3326 Views
  • 5 replies
  • 0 kudos

ADC conversion using End of Conversion Selection?

Good evening....I would like to do an A/D conversion on Channel 9 and Channel 10. I have a timer that goes off every second and within this ISR I call HAL_ADC_Start_IT. The ISR gets called upon conversion complete. Now the question is End of Conve...

SWenn.1 by Senior III
  • 5740 Views
  • 4 replies
  • 1 kudos

Resolved! FDCAN ROM bootloader pins for stm32H743ZI

As discussed in here, im trying to use ST\s ROM bootloader, when i read AN2606 Page 280 shows the FDCAN1 rx and tx Pins   Those pins dont exist in stm32H743ZI@KDJEM.1 proposed "you can activate the FDCAN bootloader with only by PH13/PH14 pins." What ...

Javier1_0-1737029159126.png
Javier1 by Principal
  • 2279 Views
  • 5 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.