STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H573 SPI clock not working

I am following a basic example from stm32: Getting started with SPI - stm32mcuI follow the steps for setting up SPI master with polling (Blocking mode). I did make sure to select the board STM32H573 DK instead of the one listed in the example.I initi...

A_Bit_More_0-1736980651955.png

DMA: last written buffer position?

DMA buffer 32 words, ADS converts 4 channels in scan mode.So every 8 ADC-starts  DMA will start at buffer[0]  (circular buffer is ticked).CubeIDE HAL is being used.How do I find out / look up  the buffer offset most recently written to?

PRenn.1 by Associate III
  • 2200 Views
  • 5 replies
  • 2 kudos

Resolved! Persistent data surviving re-programming within CubeIDE

Hi All,I'm sure this has been discussed before - and there's probably a solution out there, but for the life of me, I can't find it.So here's the situation.I have a large (~256K) block of graphics data, that sits within its own designated sectors at ...

Toneski by Associate III
  • 1351 Views
  • 3 replies
  • 2 kudos

Resolved! STM32L053 GPIO Outputs not working

Hi,We have a custom design based on STM32L053C8U8 with the pinout mapping  as image attached. The GPIOs setting and initialization code is generated by STM32CubeIDE version 1.17.0 and companion CubeMX . however, the GPIO level the output pins are not...

quanngo_0-1737057327704.png
quanngo by Associate II
  • 2922 Views
  • 8 replies
  • 2 kudos

Interrupts not working after Bootloader jump

Hey folks,I am using the STM32G0B1RE board for my development and am currently working on a Bootloader application. I have successfully implemented the jump from the Bootloader to the main application. The main application initializes correctly and e...

linker_settings.png
prateekJ by Associate
  • 1712 Views
  • 3 replies
  • 0 kudos

Resolved! HAL_I2S_TxCpltCallback is called only once

I'm testing whether HAL_I2S_TxCpltCallback or HAL_I2S_TxHalfCpltCallback is called properly by setting i2s to normal and periodically calling HAL_I2S_Transmit_DMA. However, HAL_I2S_TxCpltCallback or HAL_I2S_TxHalfCpltCallback is called only once and ...

eunoia by Associate II
  • 2943 Views
  • 7 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.