2024-11-12 5:16 AM
I have a structure that starts from my own bootloader, and I want to jump to the application. My question is similar to the one in this thread: Is it possible to keep dual bank active and executing the whole FLASH?
I am using the STM32G0B1RE microcontroller. If I put my program starting at an address in Bank 1 and continue through Bank 2, will it work without any issues?
Solved! Go to Solution.
2025-01-17 5:51 AM
I finally found related answer in this thread. Thanks for the help: Dual bank issue on stm32G0B1RCT6
So either i should disable dualbank feature or disable prefetch.
2024-11-15 5:30 AM
I plan to adjust my Flash memory structure based on the feedback I receive. If my program starts at 0x800A000 and ends at 0x801B000 (Bank1 finishes in 0x800F7FF and Bank2 starts at 0x800F800), could using both Bank 1 and Bank 2 cause any unexpected issues or behaviors?
2025-01-17 5:51 AM
I finally found related answer in this thread. Thanks for the help: Dual bank issue on stm32G0B1RCT6
So either i should disable dualbank feature or disable prefetch.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.