2025-01-16 8:25 AM
DMA buffer 32 words, ADS converts 4 channels in scan mode.
So every 8 ADC-starts DMA will start at buffer[0] (circular buffer is ticked).
CubeIDE HAL is being used.
How do I find out / look up the buffer offset most recently written to?
2025-01-16 8:35 AM
Look into DMA registers, there is a counter
2025-01-16 8:00 PM
If you use DMA and the callbacks (for Half or Full) - you should know where you are (which buffer was filled recently).
Yes, you might be able to read back also DMA registers (e.g. address pointer). Easier is to use callbacks, double buffering and knowing when DMA INT comes which buffer was (completely) written...
2025-01-17 12:19 AM
There is a macro named __HAL_DMA_GET_COUNTER(handle) that returns the number of remaining data bytes in the current DMA Channel transfer.
2025-01-17 12:39 AM - edited 2025-01-17 12:40 AM
We need to clarify some vocabulary first: Do you mean
the remaining data bytes the currently active DMA transfer still has to copy
(of a 4 conversions ADC session, 2 conversion still outstanding)
or
the remaining data bytes in the assigned DMA destination buffer (in "user" memory)
before cyclic DMA transfer will wrap back to start of buffer ?
2025-01-17 7:08 AM
It's second. Just try, making slow sampling rate (~1 sec) you can observe all processes in details.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.