STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX destroys multiple targets in Keil uVision

Posted on June 13, 2016 at 16:37Hello,I have a project with multiple targets. The project was initially generated using STM32CubeMX 4.15. I have created some targets manually. When I change some peripherals and re-generate the code, STM32CubeMX dele...

smrtkai by Senior
  • 2005 Views
  • 4 replies
  • 0 kudos

Reading value on GPIO analog mode

Posted on December 20, 2016 at 11:49Hi,could tell me someone, how to read value on GPIO analog mode (not ADC analog on AF mode). I was Googled this, and I just found that this mode has 8-bits converter. How can I recieve value from this, using HAL l...

Resolved! NUCLEO STM32F031K6 Pinout

Posted on December 20, 2016 at 10:45I'm putting together a project based on the Nucleo-F031K6 board, but I've had real trouble tracking down clear and accurate pinout definitions for the board. The first information I stumbled across was the http://...

STM32F4 - DAC start problem, when using ADC

Posted on December 19, 2016 at 11:24Hi,I do have some strange behaviour with DAC and ADC on STM32F429I-DISC0. I am using a DAC with DMA. Additionally I use two ADCs in parallel with DMA. Normally it works as expected. But when I have a voltage over ...

smrtkai by Senior
  • 2415 Views
  • 5 replies
  • 0 kudos

RTC good accuracy design

Posted on December 18, 2016 at 20:25Hello my friends.I want to design RTC board with best accuracy. My Mcu is STM32F103RB and it has Calibration option to enhance the Real Time Counter.I know 2 paramaters are so important to design: 1. Crystal accur...

st_user1 by Associate
  • 1461 Views
  • 1 replies
  • 0 kudos

Corrected clock setting from cubemx ?

Posted on December 16, 2016 at 03:20 Hello Everyone, I look forward to whom who knows Cubemx well in this community, In my generated cubemx, for GPIO initialization the code says, static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_Init...

0690X00000605rsQAA.png 0690X00000605pnQAA.png 0690X00000605t0QAA.png

Resolved! STM32F1 two byte receive with subaddress

Posted on December 17, 2016 at 16:48 I have an STM32F103 that I would like to use for I2C communication. I have been using the 'Optimized examples for I2C' with the STM32F1, but I have modified it to send a subaddress before performing the read. ...

STM32L053R8 IWDG freeze in stop mode

Posted on October 25, 2016 at 15:24Hi,I've implemented the IWDG for STM32L053R8 board and want to know if IWDG can be freezed in Low power STOP mode? I tried programming Flash option bit register, user configuration bit but still see IWDG resetting ...

STM32F417 UNALIGNED ACCESS

Posted on December 19, 2016 at 10:19HelloPeriodically, the program enters the HardFault_Handler. In the register HFSR set bit FORCED and in UFSR register set UNALIGNED.The project uses STM32F417, FreeRtos, LWIP. In most cases, the error in the stack...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.