2016-12-19 1:19 AM
Hello
Periodically, the program enters the HardFault_Handler. In the register HFSR set bit FORCED and in UFSR register set UNALIGNED.The project uses STM32F417, FreeRtos, LWIP. In most cases, the error in the stack are LWIP function. The error occurs rarely oncea few days.The program is compiled with the flag --no_unaligned_access.It is unclear why there is such an error - while --no_unaligned_access flag is enabled and even every few days, and second whether it is possible to process or ignorethis error and continue the program?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.