STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC configurations for measuring battery voltage

Posted on December 16, 2016 at 10:07Hello Everyone.I would like to infrom you that I am trying to measure battery voltage which is connected to ADC12_IN4 pin of stm32f103c8t6 microcontroller with ADC.I wrote proper code for configurations and readin...

0690X00000605tFQAQ.png 0690X00000605tKQAQ.png 0690X00000605tPQAQ.png
pm_brk_pm by Associate II
  • 2605 Views
  • 3 replies
  • 0 kudos

how i can synchronize two or more board ?

Posted on December 16, 2016 at 05:30Since I want to send data from two board to a single device which will receive data from this two board and start its processing.so how I can send this data simultaneously to another device . 

mohit rai by Associate II
  • 1329 Views
  • 4 replies
  • 0 kudos

STM32F334 24MHz+ PWM not stable

Posted on December 14, 2016 at 21:20I am having trouble getting a stable PWM of greater than 24MHz on the STM32F334 discovery board. Below are the configurations I have:8MHz external OscillatorSYSCLK = 72MHz (PLLMUL * 8MHz, PLLMULL = 9)HRTIM source ...

previn by Associate II
  • 3093 Views
  • 5 replies
  • 0 kudos

USART1 RX + DMA - stm32f030 issue

Posted on December 19, 2016 at 02:47Hello,I have an issue using the UART RX with DMA on my stm32f030k6t6...The microcontroller reacts exactly like the DMA was not correctly initialized.I'm using USART1 at PA10 (RX), and DMA1 channel 3. Here is the c...

thomas23 by Associate II
  • 966 Views
  • 0 replies
  • 0 kudos

Does STM32F446 not have full-duplex I2S?

Posted on December 02, 2016 at 04:43Hello, I am designing a project using STM32F446, hoping to get more performance than STM32F401/411.After some research and trial and error, it looks like this MCU does not support full duplex I2S. I could not find...

switch from X-NUCLEO-IDB04A1 to X-NUCLEO-IDB05A1

Posted on December 12, 2016 at 17:03HiYou recommand to switch on the board X-NUCLEO-IDB05A1 but i have the X-NUCEO-IDB04A1.You can see on my previous posts, i'm working for a package for the stm32f746g-disco.I'll be in holliday at the end of the wee...

3 Phase pwm dutycycle with DMA issue

Posted on December 17, 2016 at 11:18Hello,i am working on a school project regarding 3 phase motor control. I have a nucleo32 board with a stm32f410 deviceThe ideea is to generate a lookup table for the dutycycle values, and transfer them to the CCR...

0690X00000605slQAA.png
Bogdan by Senior
  • 957 Views
  • 1 replies
  • 0 kudos

Connecting to STM32f0 with ST-Link Utility (SWD)

Posted on January 21, 2014 at 10:36I'm having some troubles connecting an ST-Link to a STM32f0 microcontroller. Did is what i did/tried: Soldering STM32f051 (LQFP48) to DIP adaptorVBAT, VDDA, 2x VDD to +3,6VVSSA, 2x VSS to GNDBOOT0 to GNDNRST with...

r23 by Associate II
  • 3553 Views
  • 6 replies
  • 0 kudos

Processor is sensitive to moderate Temperature

Posted on December 29, 2015 at 03:33I am using the STM32F072RBT6  64pin LQFP My code seems quite stable, but this chip is showing signs of being overly sensitive to temperature... Since I have so much capacitance around the board on the same power l...

T J by Lead
  • 2035 Views
  • 6 replies
  • 0 kudos

I2C multimaster mode

Posted on December 17, 2016 at 19:28Hi,I would like to know if I can use one I2C bus for 3 devices, first is master, sencond is slave and third is master/slave (STM will siwtch between master and slave mode to communicate with this 2 devices). Is th...

karol1dw by Associate
  • 1242 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.