STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

unable to program or erase the flash

Posted on October 02, 2011 at 15:31Hi,I want to use PA13 (multiplexed with JTMS) as GPIO pin of stm32f103. So i configured AFIO_MAPR reg (SWJ_CFG[2:0] - 100 --> JTAG-DP Disabled and SW-DP Disabled) .Now i am unable to program or erase flash. Please ...

Send data 16bit over SPI using DMA

Posted on November 08, 2016 at 13:46Hi,I want to transfer data 16bit over SPI using DMA, Like thatSPI_Transmit(SPIx, (uint16_t) value, (uint16_t) count);For driver ILI9341 function clear screen faster than using SPI mode 8 bit.Many thanks.

STM32L486xx SDMMC peripheral and eMMC memory

Posted on December 01, 2016 at 16:37 Hi , I'm using STM32L486RG microcontroller and I'm trying  to use the SDMMC IP to interface with EMMC32G-M525-X01U an eMMC memory from Micron with  32Gb of size. I found in the reference manual that the SDMMC  ...

Resolved! STM32F series peripheral syntax

Posted on December 19, 2016 at 19:45Greetings,I need to come up to speed quickly on the STM32F4 series processors. I have been in embedded development for a number of years and have experience with Renesas, PowerPC, and PIC32 processors, etc and now...

IWDG with LSI on STM32L0

Posted on February 13, 2015 at 09:55Hi all,I´m trying to implement a Independent Watchdog functionality on my STM32L0.In HAL description pdf I´ve read the following sentence that give me some doubts on me:STM32L0xx devices provide the capability to ...

gerardo by Associate II
  • 1760 Views
  • 4 replies
  • 0 kudos

STM32F401 power consumption in Reset

Posted on December 14, 2016 at 20:46I'm using an STM32F401 and am trying to understand the power consumption when the device is powered (3.3VDC) and held in System Reset.  Can you tell me what the expected current draw will be when this device is he...

rwnar1 by Associate
  • 1803 Views
  • 1 replies
  • 0 kudos

STM32F072 SPI bidirectional mode strange behavior

Posted on December 13, 2016 at 10:37Hello,I'm using the STM32F072-Nucleo64 board, and direct register access (no SPL and no HAL).Using SPI in normal (aka full duplex) works without any problem, sending a byte is OK and receiving also is OK. But I wo...

Kraal by Lead
  • 2724 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.