2016-12-18 11:55 PM
2016-12-19 12:48 AM
I have carefully read this
,but I don't know what's the problem of your board.Sorry about that.2016-12-19 1:08 AM
The problem is not STM32F412G-Discovery. Problem StEmWin library. Demonstration code for this boardis written using StEmWin library. Everything works (more or less ..). But when I create a new module (window) using SWIPELIST there is a problem. As I understand it happens if SWIPELIST inherited from ICONVIEW (all your examples so made modules .. (windows) are inherited from ICONVIEW ). I think that a bug in the SWIPELIST because if it is not the error appears blank. Most likely a bug StEmWin library.. can you can somehow get around this problem? How can I use SWIPELIST using the demo code in which the parent is ICONVIEW? Question also asked on the forum SEGGER
but the answer did not get
:(
2016-12-19 10:13 PM
Here is the link to the Russian forum
http://forum.easyelectronics.ru/viewtopic.php?f=35&t=29792&p=478507#p478507
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.