2016-12-18 11:25 AM
Hello my friends.
I want to design RTC board with best accuracy. My Mcu is STM32F103RB and it has Calibration option to enhance the Real Time Counter.
I know 2 paramaters are so important to design: 1. Crystal accuracy, 2.Environment Temperature.
About the first parameter i used the Tamper pin to check the signal frequency and i found the signal frequency is 512.006Hz. So, for this frequency i used calibration Value 12.
(512.006 - 512) / 512 * 10^6 = 11.71 ~ 12 -> 12 - 11.71 = 0.281.
About this calculation i must have the lost time about (
0.281 * 86400 * 30) / 10^6 = 0.728
second per month. but after 12 days i have 12 second delay that it shows every day i have 1 second delay that means every month i have 30 seconds delay, according to the datasheet 'STM32F101xx and STM32F103xx RTC calibration' this is the value of Crystal error without calibration.This is my code to initialize RTC :
bool RTC_Init(void) {
/* NVIC configuration */ NVIC_InitTypeDef NVIC_InitStructure;/* Configure one bit for preemption priority */
NVIC_PriorityGroupConfig(NVIC_PriorityGroup_1);/* Enable the RTC Interrupt */
NVIC_InitStructure.NVIC_IRQChannel = RTC_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 1; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure);if (BKP_ReadBackupRegister(BKP_DR1) != 0xA5A5)
{ /* Backup data register value is not correct or not yet programmed (when the first time the program is executed) *//* RTC not yet configured.... */
/* RTC Configuration */
if (!RTC_Configuration()) return false;/* RTC configured.... */
/* Adjust time by values entered by the user on the hyperterminal */
RTC_Time_Adjust(defaultDate);BKP_WriteBackupRegister(BKP_DR1, 0xA5A5);
} else { /* Check if the Power On Reset flag is set */ if (RCC_GetFlagStatus(RCC_FLAG_PORRST) != RESET) { // Power On Reset occurred.... } /* Check if the Pin Reset flag is set */ else if (RCC_GetFlagStatus(RCC_FLAG_PINRST) != RESET) { // External Reset occurred.... }/* Wait for RTC registers synchronization */
RTC_WaitForSynchro();RTC_getTodayDateTime(RTC_GetCounter());
/* Enable the RTC Second */ RTC_ITConfig(RTC_IT_SEC, ENABLE); /* Wait until last write operation on RTC registers has finished */ RTC_WaitForLastTask(); }#ifdef RTCClockOutput_Enable
/* Enable PWR and BKP clocks */
RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR | RCC_APB1Periph_BKP, ENABLE);/* Allow access to BKP Domain */
PWR_BackupAccessCmd(ENABLE);/* Disable the Tamper Pin */
BKP_TamperPinCmd(DISABLE); /* To output RTCCLK/64 on Tamper pin, the tamper functionality must be disabled *//* Enable RTC Clock Output on Tamper Pin */
BKP_RTCOutputConfig(BKP_RTCOutputSource_CalibClock); #endif/* Clear reset flags */
RCC_ClearFlag();return true;
}void RTC_SetTime(DATE date) {
RTC_Configuration(); RTC_Time_Adjust(date); BKP_WriteBackupRegister(BKP_DR1, 0xA5A5);}bool RTC_Configuration(void){ /* Enable PWR and BKP clocks */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_PWR | RCC_APB1Periph_BKP, ENABLE);/* Allow access to BKP Domain */
PWR_BackupAccessCmd(ENABLE);/* Reset Backup Domain */
BKP_DeInit();/* Enable LSE */
RCC_LSEConfig(RCC_LSE_ON); /* Wait till LSE is ready */ HAL_Delay(RTC_DELAY_SET_TIME_SEC * 1000); while (RCC_GetFlagStatus(RCC_FLAG_LSERDY) == RESET){ HAL_Delay(ERROR_SHOW_TIMER); return false; }/* Select LSE as RTC Clock Source */
RCC_RTCCLKConfig(RCC_RTCCLKSource_LSE);/* Enable RTC Clock */
RCC_RTCCLKCmd(ENABLE);/* Wait for RTC registers synchronization */
RTC_WaitForSynchro();/* Wait until last write operation on RTC registers has finished */
RTC_WaitForLastTask();/* Enable the RTC Second */
RTC_ITConfig(RTC_IT_SEC, ENABLE);/* Wait until last write operation on RTC registers has finished */
RTC_WaitForLastTask();/* Set RTC prescaler: set RTC period to 1sec */
RTC_SetPrescaler(32767); /* RTC period = RTCCLK/RTC_PR = (32.768 KHz)/(32767+1) *//* Wait until last write operation on RTC registers has finished */
RTC_WaitForLastTask();BKP_SetRTCCalibrationValue(12); /* ~512.006ppm*/
return true;
}is there something wrong in my initialization...?
and another question is how can i calibrate my MCU with both parameters of '
Crystal accuracy and Environment Temperature'
...?Thanks all.
2016-12-20 2:03 AM
H
i
r
Tadayoni.S.Moham
,To find response to your question, I recommend that you refer to the application note
. For code related check , you would refer to the ready-to-use example inside the standard library (or Hal library if you would to migrate to the the STM32cube ).-Walid F'
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.