STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI slave bidirectional

Posted on August 25, 2017 at 12:09I have a difficulty with ST32F030 and Slave SPII'm trying to have it respond to an spi command:-Master sends 0x05, slave responds with an array of 7 bytes.It kind of works the first time, but then loses sync, and ge...

STM32F0308 USART set up

Posted on August 23, 2017 at 17:47 Hi, I am having trouble getting some basic USART up and running on the STM32F0308-DISCO board. I have tried both sending and receiving and don't seem to see anything coming through on either end. My code is as f...

Tom Power by Associate II
  • 6659 Views
  • 15 replies
  • 0 kudos

STM32F7 USB library supporting multi-packet mode

Posted on August 15, 2017 at 23:50Hi,I need high USB bandwidth in isochronous mode. The STM32F7 is powerful but the bandwidth depends on how the USB packet management is done.Is there a plan to support multi-packet mode in the HAL/lib/driver that co...

Resolved! STM32L433 - No JTAG Devices Found

Posted on August 23, 2017 at 22:13I'm using an ARM-KEIL ULINKPro debugger on a custom board using the STM32L433 processor. There's a JTAG connector on the board, and I'm using a TC2050-IDC-050 20:10 cable from Tag-Connect, which was recommended by t...

Migrating a project to FW_F4_V1.16.0

Posted on August 24, 2017 at 19:20I wanted to upgrade my F4 FW from 1.13 to the latest. For the STM32CubeMX Eclipse plugin to recognize the new FW I upgraded it to v.4.22.0 in the AC6 environment. I installed the F4 FW to v1.16.0 and migrated the pr...

Ron Koch by Associate II
  • 1553 Views
  • 1 replies
  • 0 kudos

HAL_UART_Receive_IT,continuous reception

Posted on August 23, 2017 at 01:28Hello, i'm using STM32F103c8t6 and i'm on a project where i have to send 8 bytes from an MCU to another in a asynchronous way , so i used HAL_UART_Receive_IT() , but i remarked that the HAL_UART_RxCpltCallback() is ...

sak hos by Associate III
  • 2939 Views
  • 3 replies
  • 0 kudos

Nucleo-f070rb bootloader

Posted on August 24, 2017 at 19:45My board is connected with usb-ttl board and I can communicate with uart using HAL drivers.  I am trying to connect using STMFlashLoader Demo app from ST but I keep getting No response from the target,...So far I ha...

Ran Kai by Associate II
  • 932 Views
  • 0 replies
  • 0 kudos

How to tone down a signal in ST board?

Posted on August 24, 2017 at 17:56Hi community,A lot of sensors output go from 0 to 5V. But the ADCs on Nucleo Boards have a 0-3.3V range. The solution is to use some external resistors to reduce the input of the ADC.Is there another solution withou...

S25FL127S QSPI problem with STM32F746

Posted on August 13, 2016 at 01:07Hello ST Forum,I have a problem related to the QSPI with STM32F7xx, details as the following:I have a STM32F746G-DISCO board, I run on it he code “QSPI_ReadWrite_IT�? found in “STM32Cube_FW_F7_V1.4.0�? the results w...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.