2017-08-24 8:56 AM
Hi community,
A lot of sensors output go from 0 to 5V. But the ADCs on Nucleo Boards have a 0-3.3V range. The solution is to use some external resistors to reduce the input of the ADC.
Is there another solution without external resistors? I think using 5V tollerant pin, then route the signal somewhere that could tone down the signa and then enter in ADC. Is it possible?
I think about OPAMP but I notice that I can only amplify the signal.
What do you think?
#attenuator #adc2017-08-24 9:25 AM
Most sensors are high impedence while the ADC requires low impedence, hence an external op-amp with voltage scaling would probably be effective. Using sensor with lower operating voltage be a plus. Ideally, differential sensors with differential input ADC on STM32 may provide better common mode noise reduction.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.