2017-08-25 3:09 AM
I have a difficulty with ST32F030 and Slave SPI
I'm trying to have it respond to an spi command:-
Master sends 0x05, slave responds with an array of 7 bytes.
It kind of works the first time, but then loses sync, and get OVR bit set. I can't figure out why.
Heres the code:-
int main(void)
{HAL_Init();
/* Configure the system clock */
SystemClock_Config();/* Initialize all configured peripherals */
MX_SPI1_Init();spi_init();
while (1) { HAL_SPI_Receive_IT(&hspi1, &spiData[0], 1); }}
/* SPI1 init function */
static void MX_SPI1_Init(void){hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_SLAVE; hspi1.Init.Direction = SPI_DIRECTION_2LINES; hspi1.Init.DataSize = SPI_DATASIZE_8BIT; hspi1.Init.CLKPolarity = SPI_POLARITY_LOW; hspi1.Init.CLKPhase = SPI_PHASE_1EDGE; hspi1.Init.NSS = SPI_NSS_SOFT; hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi1.Init.TIMode = SPI_TIMODE_DISABLE; hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi1.Init.CRCPolynomial = 7; hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE; hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;/* SPi priority interrupt configuration */
HAL_NVIC_SetPriority(SPI1_IRQn, 1, 1);if (HAL_SPI_Init(&hspi1) != HAL_OK)
{ Error_Handler(); }}
void SPI1_IRQHandler(void)
{ HAL_SPI_IRQHandler(&hspi1);}uint8_t spiData[8];
uint8_t edgesmsg[7];
void spi_interrupt()
{ uint8_t c; c = spiData[0];if ( c == 0x05)
HAL_SPI_Transmit(&hspi1, edgesmsg, 7, 1000);}
Any suggestions gratefully received..
#spi #slaveWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.