STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USBLC6-2SC6 ESD wont protect

Posted on August 24, 2017 at 09:47HiWe have a device which is an USB powered(USB2.0), and on the same USB port is the communication with the PC.So it is powered from the PC.For the ESD protection of the USB lines we add the USBLC6-2SC.Our processor ...

0690X000006080EQAQ.png

Resolved! STM32F746 QSPI strange behavior

Posted on August 22, 2017 at 04:23I'm experiencing strange behavior of QSPI peripheral (or may be flash chip itself -- N25Q128 in SO8; chips are not shiny new, but never used; datasheet Rev. 8 July 2014): despite what is stored in NVCR/VCR registers...

enable mac receive all

Posted on August 24, 2017 at 16:11Is it possible to configure mac init as enable with cubemx, until now, it is always disable?macinit.ReceiveAll = ETH_RECEIVEAll_DISABLE;

STM32F0 CAN Stops communication

Posted on August 16, 2017 at 21:39Hello,I'm working with STM32F0 and CAN communication, sometimes the CAN peripheral stops, doesn't send or receive messages.In the past I asked the same issue and the answer was that it could be the HAL_LOCK funtion ...

eng23 by Senior
  • 4927 Views
  • 12 replies
  • 0 kudos

ADC1&3 w/ext trig, bad code from CubeMX w/NucleoF303ZE

Posted on March 27, 2017 at 14:15Start with new CubeMX project, selecting NucleoF303ZE board. Enable 1 single ended channel on each of ADC1 and ADC3. Select Regular Conversion Trigger for both. CubeMX generates this line in MX_ADC3_Init():  hadc3.In...

PA9 as VBUS sense of USB_OTG_FS (STM32F407)

Posted on August 24, 2017 at 15:33I played with PA9 on a DISCO-F4 board in its OTG_FS_VBUS function. This is a non-AF function, i.e. it's connected to PA9 all the time, and is supposed to be governed by USB_OTG_FS settings. I am not interested in OT...

STM32F7 HAL CAN Receive interrupt only once

Posted on January 25, 2017 at 20:33I seem to have an issue with receiving CAN messages.  It is set up on an interrupt, but the interrupt only seems to fire once, and when I receive the 2nd message, nothing happens.  There seems to be very little on ...

STM32L443 microcontroller wake up problem

Posted on August 24, 2017 at 11:00Hello,   I'm working on a project where I need to shut down my device, when it finished it's task. I use an STM32L443 microcontroller to control the device. The circuit was designed, that if happens a falling edge o...

STM32F4 UART 16 bits speech data sending?

Posted on August 21, 2017 at 14:58I'am trying sending speech data between two STM32F4 board with. I take speech data from PCM buffer. But the data that in PCM buffer is 16 bits. I need to send this data with UART. I know that, UART data register is ...

H. Kartal by Associate II
  • 5405 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.