STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bootloader + Two applications

Posted on September 07, 2017 at 08:19Hi, I have to download second application and enter second application from the first application.Bootloader to First application jump is happening and working fine.I have problem to jump to second application fr...

Resolved! Maximum output current value of PWM, TIM

Posted on September 16, 2017 at 18:18Sorry for my poor English.What is the maximum output current value of PWM using TIM? Where can I find it in the data sheet? I am using STM32F334. I am investigating whether the MOSFET can be directly driven by th...

0690X00000608GvQAI.png
Ken Inoue by Associate III
  • 2087 Views
  • 4 replies
  • 0 kudos

Freeware compilers for STM32 family ?

Posted on May 05, 2017 at 04:02I am new to the STM32 world.   I've played a lot with many 8051 varieties and now want to expand.   I am thinking of buy a few of the really simple STM32 boards to play with, and just start writing code from scratch.I'...

STM32F100: Problem reading sensor via I²C

Posted on July 29, 2015 at 13:47 Hello, I am new to STM I started with the STM32100E-Eval Board which features an STM32F100Z3 MPU and a STLM75 temperature sensor, which connects to the MCU via I²C2. Using STM32CubeMX, I set up th...

pascal23 by Associate
  • 2004 Views
  • 3 replies
  • 0 kudos

STM32F765 FatFs, SDIO, DMA, FreeRTOS HAL 1.8.0

Posted on September 15, 2017 at 23:53I have been struggling for a week now trying to get FatFS working over the SDIO under FreeRTOS.  I was making some progress debugging through the HAL but I have come to a difficult part to debug.While debugging t...

Stephen28 by Associate III
  • 1170 Views
  • 2 replies
  • 0 kudos

HardFault and working reverse GPIO Pins

Posted on September 14, 2017 at 15:12 Hi friends, I've got problems with STM32F0 series also same F1 now my real problem is getting a HardFault ,when I try to work with Nrf24lWhen process arrive this line 'TM_NRF24L01_SetTxAddress(&hspi1, TxAddres...

Zek_De by Senior
  • 4379 Views
  • 12 replies
  • 0 kudos

[OTG + documentation + Cube] OTG_HS_GUSBCFG.TRDT values

Posted on August 29, 2017 at 23:06In RM0090 rev.15, OTG_HS_GUSBCFG.TRDT description (p1410) links to Table9, which gives a single value, 0x09.However, in CubeF4, the TRDT value is determined based on the actual link speed (regardless of whether inte...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.