STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to enable generation of HAL_NAND_MspInit()

Posted on September 17, 2017 at 17:46Hi,The HAL_NAND_MspInit() is not generated in the stm32f4xx_hal_msp.c when the attached .ioc is used. Therefore the NAND pins are not driven by the MCU and NAND driver is not working at all. How can I enable gene...

STM32 digital input frequency

Posted on September 18, 2017 at 17:58Hello, my problem is I need to acquire a waveform at high frequency (sampling frequency in the order 35 to 50 MHz carried out by fast external ADC). I would like to use an high performance STM32 microcontroller (...

Parsing ETH/RS232<->CAN

Posted on September 18, 2017 at 16:31Hi community,i have following situation:PC <--- ETH or RS232 ----> STM32F107 < ----CAN---- > STM32F105 with external power moduleI want to parse the ascii message (example K01NC|200) to a smaller protocol what i ...

sprintf function does not work in keil compiler

Posted on September 15, 2017 at 22:38Hi to allI am new in STM32 and keil (I used Atmel chips) and now I am getting familier with them.I made a project and I can send data to serial port with the following function :'HAL_UART_Transmit(&huart1,(uint8_...

STM32L072RBT6 minimum voltage for USB device

Posted on September 11, 2017 at 21:20Can it work as USB device on 1.8V (VDD), with separate regulator for 3.3V on VDD_USB?How pulling of D+ over 1.5k to 3.3V is done (internaly maybe)? If there is other performance limitation regarding working on lo...

Can I use stm32f407 for smartcard project ?

Posted on September 18, 2017 at 11:06Hi, Can I use stm32f407 for smartcard project ? I found prepared smartcard project for some EVAL boards and STM32L053 boards in st's website. I wonder that can stm32f407 be used instead of eval boards and l053 bo...

Resolved! display address CCM

Posted on September 15, 2017 at 17:52Hi,I try to move some array in CCM on stm32f415.I modify the ld script with  CCM_SRAM   (rwx) : ORIGIN = 0x10000000, LENGTH = 64K .ccmram : { . = ALIGN(4); _sccmram = .; /* create a global symbol at ccmram start ...

OA1ZHA / TSZ121 precision amplifier

Posted on September 16, 2017 at 12:33I'm not sure if I'm understanding the gain bandwidth correctly, but can I use OA1ZHA op amp for a signal with ADC sampling frequency of 2 kHz? or am I really limited to only 400 kHz based on maximum gain bandwidt...

0690X000006045dQAA.jpg
Kevin A by Associate
  • 1280 Views
  • 1 replies
  • 0 kudos

Output control Question

Posted on September 18, 2017 at 02:59EX) ODR = 1   -> I/O Pin State = 0 ?It is True?If ODR = 1 then I / O port is also 1?Is it OutputControl Not Gate?

0690X00000608HJQAY.png

Update from F4 to F7 -> Performance Problems

Posted on September 15, 2017 at 14:17Hallo everybody,i have a circuit board whitch is fitted with a STM32F429BIT.The Software use STemWin and LWIP (without RTOS) and works good.Now i has order the same circuit board with the pin compatible STM32F767...

mfrank9 by Associate III
  • 815 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.