2017-05-04 7:02 PM
I am new to the STM32 world. I've played a lot with many 8051 varieties and now want to expand. I am thinking of buy a few of the really simple STM32 boards to play with, and just start writing code from scratch.
I'd like to ask what people would recommend as far as a freeware compiler goes ?
Thanks2017-05-05 1:42 AM
Hi
mcuny
,I recommend you to use the
.This way, you will benefit fom the already available examples ready to use with this toolchain that are available in the STM32Cube package.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2017-05-05 2:13 AM
For most of the freeware packages, the launchpad compiler at
https://developer.arm.com/open-source/gnu-toolchain/gnu-rm
is the original source of the toolchain. If you need the bare toolchain, consider the link above.
2017-05-05 2:27 AM
If you don't like/need the Cube approach (see other threads here), I can recommend EmBlocks (now called EmBitz), a free gcc-derived toolchain with an IDE based in CodeBlocks. It supports the 'old' Standard Peripheral Libs, but no Cube.
2017-05-05 4:35 AM
I use GNU/GCC, works fine.
Keil is free for Cortex-M0 STM32 parts.
2017-09-17 8:51 AM
It is really easy to import CubeMX generated project into EmBitz.
2017-09-17 9:28 AM
Create a project from scratch (the lowest start) - it's very difficult. It can be said - almost impossible. This is tantamount to designing an atomic reactor for a comic liner. You will surely stumble, and for a long time you will look for the cause.
You need examples to follow. Such simple and as your task.EmBitz has a starting configuration in a similar style. Nothing superfluous is the minimum. It is enough for communication through the debugger to edit the contents of the processor registers in real time.Everything else becomes available in the programming process.I advise you to divide the program into two levels: iron and code. Otherwise it will be very difficult. The program for iron will have to be written for each project. Exceptions do not exist. Each new project is a unique task, the program for iron can not coincide.
The algorithms for C are universal, this code can be easily reused. And most importantly - use someone else's code.
Use the turtle (version control)
https://community.st.com/external-link.jspa?url=https%3A%2F%2Ftortoisehg.bitbucket.io%2F
- this will help in development.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.