STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeL4 1.9.0 CubeMx 4.22.1

Posted on September 14, 2017 at 22:45There might be an ADC clock issue when the project is configured with CubeMx 4.22.1 and 1.9.0 CubeL4.When SAI clock is selected for ADC in CubeMx the HAL_RCCEx_PeriphCLKConfig called by SystemClock_Config returns...

ax0018 by Associate III
  • 745 Views
  • 1 replies
  • 0 kudos

STLink-V2 VCP @ 115,200

Posted on July 10, 2017 at 23:40I'm running into an issue with the STLink-V2 VCP when transmitting TO the dev board at 115,200. It is suspiciously similar to this old post, except in the opposite direction: https://community.st.com/0D50X00009Xkh6hSA...

jcsoo by Associate II
  • 6247 Views
  • 8 replies
  • 0 kudos

ST-LINK VCP with flow control?

Posted on September 14, 2017 at 23:01The newer version of ST-LINK (intended for mbed) supports on several boards, e.g. STM32F4 DISCO1, the UART as USB VCP (ST-LINK chip acts as the USB UART bridge, e.g. Tx/Rx going to UART1 on the MCU).It works fine...

Is there a USB HID example not using CubeMX

Posted on September 15, 2017 at 07:00Hi   I am about to select a STM32L0x device with USB , and trying to find an example on how to use it as a HID . I want to connet the device to a PC where I can communicate with it via a Windows application I hav...

Reliable U(S)ART between two STM32 MCUs with internal oscillator

Posted on September 15, 2017 at 11:37Hello!I have a best practice question.Correct UART communication requires the transmitter and receiver clocks differ by less than 5% (2.5% per MCU), otherwise communication errors may occur. For the temperature r...

0690X00000608FrQAI.png
T B by Associate II
  • 1646 Views
  • 2 replies
  • 0 kudos

2D Array in Struct

Posted on September 15, 2017 at 14:57HelloI could not define a 2D array in a struct with Keil Compiler. How do you do that? Does anyone have information? 

How to start the ADC in STM32F746NGH6 Discovery

Posted on September 15, 2017 at 16:15Has somebody an easy solution for starting a basic ADC conversion in STM32F746NGH6 CPU. ADC3 channel 8 would be good because that is connected out. Without HAL because I have tried to combine a HAL version and an...

LMI2 by Lead
  • 611 Views
  • 0 replies
  • 0 kudos

STM32F429 LIN usage

Posted on September 14, 2017 at 13:57Hi all, I have a problema using STM32F429 USART Hal functions in conjunction with a LIN device, using USART1.I configure the peripheral as any other UART in the project, using a pattern like:LinPinInit(){   ...} ...

stm32f429zi_interrupt_register init qusetion

Posted on September 15, 2017 at 06:58CUBE MX Basic Settings (STM32F429ZI)and My code...int main(void){  /* USER CODE BEGIN 1 */  /* USER CODE END 1 */  /* MCU Configuration----------------------------------------------------------*/  /* Reset of all...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.