STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32C031C6 I2C error handling

I am using STM32C031C6 MCU connected to an NTAG5 IC via I²C. The MCU is configured as an I²C master transmitter and master receiver. Polling mode is used to transmit and receive data to/from the NTAG5.Below is the code I am using to write and read I²...

arti_0-1740444824068.png arti_1-1740445145026.png
arti by Associate
  • 731 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H7S78 USB CoreReset timeout

Hey All, Similar issue to this previous topic,I'm running into a timeout error every time I try and call  USBx->GRSTCTL |= USB_OTG_GRSTCTL_CSRST from the USB_CoreReset function in the example code. It seems like the previous solution was to make sure...

halfordC by Associate II
  • 4021 Views
  • 5 replies
  • 4 kudos

How to configure GPDMA for PWM generation?

Hi,I'm using a Riverdi RVT50HQSFWN00 Screen with the STM32U5A9NJH6Q MCU. COnnected to pin PI0 is a WS2812 LED light strip. I already configured the timer 5 channel 4 for PWM generation and validated it with a scope at the pin. Right now I'm stuck at ...

m4rk0401_0-1736341234347.png m4rk0401_1-1736341318843.png
m4rk0401 by Associate II
  • 2527 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F429: CAN cannot receive messages

I am trying to use my STM32F429IGT6 CAN to receive some data from the host computer. The data is basically 4 16-bit unsigned integers (8 bytes in total), the message ID is 0x16 and uses the 11-bit standard ID format. The host computer sends messages ...

most1ma by Associate III
  • 14081 Views
  • 25 replies
  • 1 kudos

FMC with NAND Flash 8 times slower than expected

I am evaluating NAND Flash as a means of storage for a product. I am using the Toshiba TC58NVG1S3HTA00 and using it with the FMC on the NUCLEO-U575ZI-Q board. While I have established comms and have been able to read, write and erase the flash chip s...

FMC Registers.png TotalMessage.png ZoomedIn.png

ARR update causing output glitch

Using STM32F765, I'm using tim1 with OC toggle.The issue is glitches when I update the ARR value within the Repetition UP ISR.  ARR Preload is enabled, not sure what to look at here.D2 toggles when the TIM1_UP_TIM10_IRQHandler fires, and D3 is TIM1 C...

Screenshot 2025-02-26 14.23.59.png
_EFrie by Senior
  • 1687 Views
  • 4 replies
  • 1 kudos

STM32H5 external loader

Hi, I need the project used to generate the external loader: MX25LM51245G_STM32H573I-DK.stldr. My custom board uses a STM32H563VIT6 and the same octo-spi flash from Macronix used in the STM32H573I-DK board. But with different gpios connections. So th...

AMend.7 by Associate III
  • 38425 Views
  • 60 replies
  • 7 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.