STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FW flashing from Bootloader

Hi , I am now working on FW upgrade using uart . Bootloader receives the application hex file through uart and flashes it .Then jumps to application , but facing some issues with flashing , flashing is not taking place. I am using NUCLEO-H723ZG board...

CJ007 by Associate III
  • 3392 Views
  • 5 replies
  • 1 kudos

ADC conversion speed /sampling rate

Hi, I am working on the STM32L476RG MCU, where I convert a 3.3V ramp signal into a 0 to 360-degree angle using a 12-bit ADC. After that, I generate a digital signal using a GPIO pin. However, I realized that up to 1 kHz of ramp analog input, it works...

Resolved! VBUS Sensing STM32F107RCT6

Good morning,I am implementing a USB connection between my PC and the STM32F107 MCU in Device Only mode on a custom PCB. Since the PCB is powered through the USB connector (VBUS), I do not want to use the VBUS sensing pin (PA9) to activate USB commun...

Immagine 2025-02-14 024647.png

STM32G030C8T6 LED blink not working

Hi everybody,I am having a problem with stm32g030c8t6 as follows:I tried to write a draft program to blink the led, when I debug, the ODR register blinks but my Led does not blink. I checked on the PD0 pin and found that there is no signal output. Pl...

Resolved! OpenOCD and RDP protection [STM32g0x]

Hi everyone I'm currently trying to set RDP option bytes on STM32G070 chip with OpenOCD I try :> reset halt [stm32g0x.cpu] halted due to breakpoint, current mode: Thread xPSR: 0xf1000000 pc: 0xfffffffe msp: 0xfffffffc > stm32g0x lock 0 flash write a...

STM32L053, using DAP

hi I am currently using STM32L053 processor and ST LINK debugger with KEIL MDK5. For printing Assert condition I require DAP. (Don't want to use serial port.)For that as I read, will need to use Event recorder . As my processor has M0 core need to ch...

Resolved! AN4221 - Confusing instructions for Read Memory command

Previously I posted a message thinking that there was an error in AN4221 regarding the checksum and whether it should be complemented.  However, looking at (for instance) the Write Memory command, I can see that the command byte sequence and the data...

dmarks-ls by Associate III
  • 1386 Views
  • 1 replies
  • 0 kudos

Resolved! CAN AND UART STM32F446RE

    HAL_UART_Transmit(&huart2, (uint8_t *)"UART OK\r\n", 9, HAL_MAX_DELAY); filter_config(); if (HAL_CAN_ActivateNotification(&hcan1, CAN_IT_RX_FIFO0_MSG_PENDING | CAN_IT_BUSOFF) != HAL_OK) { HAL_UART_Transmit(&huart2, (uint8_t *)"CAN Notificatio...

Yakry by Associate II
  • 2996 Views
  • 6 replies
  • 3 kudos

STM32H7S3L8 LL DMA USART TX transfer

Hi,I want to setup USART3 TX transfers using GPDMA, however, without success.For such purpose I also followed this article: https://community.st.com/t5/stm32-mcus/how-to-configure-the-gpdma/ta-p/49412STM32CubeMX setup is:USART TX DMA ChanThe code for...

simozz_0-1739974981911.png
simo zz by Senior II
  • 1401 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.