STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Memory Synchronization Barriers

I am running code on an STM32U585QI that enters STOP2 when the code is idle.   I am disabling the data cache before going to stop2, and enabling it when coming out (to deal with an errata item).  My code basically does this:HAL_DCACHE_DeInit(); HAL_P...

BDoon.1 by Associate III
  • 2638 Views
  • 4 replies
  • 1 kudos

Resolved! STM32L476 OPAMP is not working as expected

Hi,I am using an STM32L476 on Nucleo64 board, I am amplifying a 1MHz 200mVpp sine wave with a 100mV offset in order to try the OPAMP but I dont think it is working. I configured OPAMP in PGA not connected mode(Also tried PGA connected too) and gave i...

Stm325_0-1742476994977.png Stm325_1-1742477009544.png PGA2_CON.PNG
Stm325 by Associate III
  • 1773 Views
  • 2 replies
  • 0 kudos

Resolved! ADC different channel, same value

    I am just wondering how it is possible that 3 adc gave me the very same value, if I change the channel and their rank are different.   Thanks for all.   

carlesls2_3-1742472404962.png carlesls2_4-1742472418135.png carlesls2_5-1742472436041.png
carlesls2 by Associate III
  • 1794 Views
  • 4 replies
  • 1 kudos

Resolved! ADC1_IN16 (no mode)

I begin a new project I want to use the PA12 as a ADC input. But the pin is orange and I am unable to activate the mode or channel of the ADC.What is the explanation behind it? How do you explain it?Thanks a lot to all. 

carlesls2_0-1742466439720.png carlesls2_1-1742466529049.png
carlesls2 by Associate III
  • 1285 Views
  • 2 replies
  • 1 kudos

STM32L476 Changing VRef for ADC precision

Hi I want to sample low voltage signals with STM32L476 so I figured it would be a good option to reduce reference voltage and I found this part in the MCU datasheet: Now I am using ADC in dual mode and sampling 8 bit so it is not too precise for low ...

Stm325_0-1742410285083.png Stm325_1-1742410285211.png
Stm325 by Associate III
  • 2050 Views
  • 5 replies
  • 0 kudos

adding CMSIS-DSP library to stm32h743

hi,I want to use CMSIS-DSp library in my stm32h743 project. the project contain USb MSC device also.After adding the library to project i am getting 5 errors, which I am listing below,11:56:50 **** Build of configuration Debug for project DIN_MAIN_V3...

ykn by Senior
  • 1153 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.