STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Abnormal GPIO Operating Frequency on STM32H743IIT6

Dear Support Team,I am encountering an unexpected issue with my STM32H743IIT6 microcontroller where the GPIO operation frequency observed via an oscilloscope is only ​16.6 MHz, despite configuring the ​bus clock at 400 MHz and ​AHB clock at 200 MHz. ...

nhong by Associate
  • 1270 Views
  • 2 replies
  • 2 kudos

Resolved! QSPI external RAM

hi all,i was trying to work with stm32u585 microcontroller and an external RAM IS66WVQ2M4DALL , which is a QSPI based RAM can work in 133Mhz.the RAM support DDR based data transfer. Here i am attaching my OSPI configuration  hospi1.Instance = OCTOSP...

sabari1_0-1738740509990.png
sabari1 by Associate III
  • 4860 Views
  • 10 replies
  • 1 kudos

Resolved! How to update firmware over USB C

Hi,My board with a STM32F745VEH6 is working as a device, that need to be updated via USB C over time. How can I do that? Is there a way to update the firmware with command line?I tried to connect the micro over USB C with STM32CubeProgrammer, and got...

MF_GS_0-1742413158174.png
MF_GS by Associate
  • 2174 Views
  • 3 replies
  • 1 kudos

Resolved! STM32L476 Interleave and opamp

Hi, I am sampling high rate data using STM32L476 in Nucleo64 board in dual channel interleave mode. I am measuring very low voltage values so is it possible to use MCUs internal opamps together with interleave mode. It looks like I am not able to act...

Stm325 by Associate III
  • 2083 Views
  • 4 replies
  • 0 kudos

Functional Safety

Hi everyone,I need functional safety data for STM32G473VET6. (FIT value or MTTF value or MTBF value or λ value). How can I get these values?Best Regards,

Fd202006 by Associate
  • 1261 Views
  • 2 replies
  • 1 kudos

Resolved! HRTIM Burst Controller HELP

Hello everyone,I need to implement the burst controller in HRTIM in order to load 3 compares of the master timer at once.I am using low layer so I do not have a lot of info.My .ioc setting are:Then, in the DMA CH1 interruption I have something like t...

PMoreno_0-1740752846323.png PMoreno_1-1740752880323.png PMoreno_2-1740752892087.png
PMoreno by Associate II
  • 2033 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.