STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Audio Device Class simple example with STMStudio

Posted on June 22, 2018 at 13:36 Hello, I'm trying to make STM32F3Discovery as an USB audio device. I want to stream audio to variable and use STMStudio to display graph for audio data. Later I want to feed PWM and control D amplifier. Pinou...

0690X0000060PGhQAM.jpg 0690X0000060PGiQAM.jpg 0690X0000060PGoQAM.jpg 0690X0000060PGXQA2.jpg

Debugging crashes at the middle of the program

Posted on June 21, 2018 at 10:35Hi All. I am using:IDE: System  WorkbenchBoard: Nucleo L476RGMCU: STM32F031G6U6At first debugging starts without any issues. But then at some point in the program I get the error No source available for '0x1fffedba' I...

NFC Byte address issue

Posted on June 12, 2018 at 09:37HelloI am working with  M24Sr02 NFC module and interfacing it to STM32R0F8 controller in my project. The code has been generated using CubeMX. The data send and receive functions used show SUCCESS but the data i recei...

Incorrect low power current consumption CMWX1ZZABZ

Posted on June 21, 2018 at 16:03Hello,I design a LoRa aplication with CMWX1ZZABZ module. The schematic which I use is the following:And the current consumption es 1.2mA. Anybody know which are the errors in the schematic to get 1.65uA of the datashe...

0690X0000060LMZQA2.png

Resolved! DMA priorities for LTDC

Posted on June 22, 2018 at 08:57Hi,I have a problem with configuring priorities for DMA channels and LTDC controller.I am using a DMA channel to communicate with a DSP processor. In this channel I need a large data transfer. When I start the DMA cha...

Need I/O controller EVM board

Posted on June 05, 2018 at 06:30 Hi there, I have been back to high power design. My system contains 3phase, 380V, 50Hz ac input, secondary surge protector, Aux Tr ( single phase, 380V/220V, 300VA), phase transformer( 3ph, 380v/12v,0v,12v,100VA...

Resolved! CubeMX I2C Configuration issue with STM32H753IIKx

Posted on June 07, 2018 at 12:55Hello,I've created new STM32H753IIKx project with CubeMX(Ver4.26.0), and changed the I2C1/I2C2 setting into 'I2C' from 'Disable' in Pinout tab.And, switch to Configuration tab, open the I2C1 Configuration, move to GPI...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.