2018-06-12 12:37 AM
Hello
I am working with M24Sr02 NFC module and interfacing it to STM32R0F8 controller in my project. The code has been generated using CubeMX. The data send and receive functions used show SUCCESS but the data i receive back is not exactly equal to the one sent. Functions used are 'M24SR_SendI2Ccommand' and ' M24SR_ReceiveI2Cresponse'.
Can anyone tell me where do we write the byte address where the sent data has to be written?
The SendI2C command calls another function ' HAL_I2C_Master_Transmit(&hi2c1,I2C_WRITE, (uint8_t*)pBuffer,NbByte,1) ' . Where is the byte address specified over here ???
2018-06-22 1:50 AM
Hi
sardaparakh
,The M24SR (in contrary of other nfc memories) has specific commands for the I2C communication, these commands are similar to the RF commands using the NFC Forum Type 4 or ISO14443A format like I-block or APDU. I would recommend you to read the M24SR
https://www.st.com/resource/en/datasheet/m24sr02-y.pdf
if you do not have already did it.Also note, that before reading or writing to the memory you will need to open a session (select application and select NDEF file ... as same as for a reader). This memory cannot be accessed like a standard EEPROM.
So to answer your question, you have to inform the destination address in the C-APDU command 'update binary' (detailed in the DataSheet) that you need to build and insert in thepBuffer parameter of HAL_I2C_Master_Transmit.
To help you, you can consult some example codes available on st.com in the
package. This software is supplied with the Nucleo extension board which includes our M24SR chip.Best Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.