STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Pin Remapping Confusion

I am using the STM32G071. My first board is built on the G071G8UxN. This is a 28-pin version. UCPD1_DBCC2 on pin 14 PB0UCPD1_DBCC2 is also on PA10 but that's not connected on the 28-pin version. However, you can remap and replace PA12(pin 19) with PA...

Carl_G by Senior III
  • 1129 Views
  • 1 replies
  • 0 kudos

Resolved! STM32U5 - achieving low power (micro ampere range)

Hi,We are currently utilizing a custom-designed STM32U5G7 microcontroller for our application with the MSI clock configured to 1 MHz. Despite configuring the device in Sleep and Stop modes, with all GPIO pins set to input and one pin configured as an...

_Danny__0-1743056824480.png _Danny__1-1743056858029.png _Danny__2-1743056957591.png
_Danny_ by Associate III
  • 1560 Views
  • 2 replies
  • 2 kudos

Resolved! ADC STM32H743

We use a STM32H743 and I want to connect an external reference voltage to the Vref pins. We use 3 ADCs, and for each ADC, we sample 4 channels. Each channel must be read at 100 ksample/s. The 3 ADCs operate continuously. A common ADC clock of 10 MHz ...

mswart by Associate
  • 1182 Views
  • 1 replies
  • 1 kudos

Couldn't get any ADC value with STM32H573 ADC

I need help. I couldn't get any adc value whether with live expressions or UART . UART is working fine so the problem is within the ADC configuration code. have i miss or overcomplicated anything?   #include "stdio.h" #include "stdint.h" #include "st...

B.Redmoon by Associate II
  • 1369 Views
  • 2 replies
  • 0 kudos

Resolved! Problem with USART on Nucleo-F401RE

Hi, I am pretty new to STM32 MCUs and I am having trouble with USART communication. I would like to send a message from Nucleo-F401RE to raspberry pi 3b+, and then to display that message in terminal on raspberry. I have tried to use USART2 for this ...

david027 by Associate II
  • 1445 Views
  • 1 replies
  • 0 kudos

STM32H755 dual ADC DMA timer trigger

Hi,I'm using STM32H755ZI-Q Nucleo board and I'm trying to use TIM2 to trigger Dual ADC conversion. M7 core is running FREERTOS and M4 is bare metal. ADC is controlled by M4 core. DMA is used to transfer data to M7 and then M7 is using ethernet to tra...

ADC1.PNG clock2.PNG DMA.PNG interrupt.PNG
mosamasa by Associate II
  • 1224 Views
  • 2 replies
  • 0 kudos

Resolved! USB data toggling with DMA

Hey folks,I've seen many posts from frustrated users of USB OTG HAL, especially when enabling DMA. I created a fix for data toggle errors (DTERR) when using DMA with USB_OTG_HS HCD paired with full speed embedded PHY on a STM32F4xx.  Hopefully this f...

skeeter by Associate II
  • 2324 Views
  • 4 replies
  • 4 kudos

Log Data coming from MZ-AI Kit

Moved from Feedback Forum. The Feedback Forum is not for product questions. Hello everyone, I started working with STM32 devices a few weeks ago. Currently, I'm dealing with the VL53L8CX sensor and the MZ-AI kit. Since I have a Linux PC (Ubuntu)...

kgb by Associate III
  • 1386 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.