2025-03-31 3:47 AM
what is the best/easiest way to have multiple connections to the same debug target using stlink as a debug adapter, i mean during an active debug session within the cubeide have another PC tool (custom built) that can interract with the hw, like read/write memory and registers.
Theoretically the stlink can be shared via the stlinkserver, however its usage is not well documented (or at least i'm not aware of it)
Some possibilities i could think of:
1. talk to the stlinkserver directly somehow
2. next to the active gdb connection from cubeide have a telnet session from the other tool
3. use 2 instances of openocd, one from cubeide and the other for the tool (gdb based)
4. others?
I would prefer gdb based solution. Performance is relevant as i need to transfer large amounts of data
Any hints, ideas?
2025-04-01 7:15 AM
What are the "multiple" tools that need to talk to your device?
2025-04-02 12:10 AM
as i mentioned in the original post, the main tool is the cube ide, and the other one is a custom built one, it doesn't exist yet, just a proof of concept to evaluate what would be the best way to do this, but if someone already did something similar, or if there is a recommended way to do this, that would be helpful.
So far i tried 2. and 3. both of them work, i need to evaluate from performance point of view which one is better, i don't think it is worth messing with 1. as it is not documented and i don't think it is meant for 3rd parties.
2025-04-03 3:11 AM
of course i had to mess with 1. i just pulled out the hla and stlink_usb files from the openocd project and put it in my project, now i can talk to the stlink server directly, the hla interfaces are exactly what i need, so this method also works, i have a feeling that this is the most performant way to do this, no middleman, just talk to the stlinkserver directly, openocd source is a good enough documentation for this. the hla driver is pretty much plug and play
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.