STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI Clock Signal Configuration

Hi everyone,I’m encountering problems with SPI communication with the board NUCLEO-H753ZI and the EVAL-AD5764 from Analog Devices, as this is my first time working with it, and I’m unsure if I’ve configured it correctly.I’ve consulted a forum for Ana...

JonConesa_0-1742906278662.png JonConesa_1-1742906346384.png JonConesa_2-1742906373032.png JonConesa_3-1742906390060.png
JonConesa by Associate III
  • 2401 Views
  • 4 replies
  • 0 kudos

how to configure the bluetooth for b-l475e-iot01a

Hello, i'm trying to communicate with my b-l475e-iot01a with the bluetooth. In the documentations i don't see nothing about configuration and i don't know how to configure the bluetooth.I don't know how to make the board visible. Someone can help me ...

MMari.5 by Associate II
  • 2800 Views
  • 5 replies
  • 0 kudos

STM32G0 ADC channels availability and GPIO mapping

Hi There, I am currently using the STM32G050C8T6 (LQFP48) and would like to use PA11 as an ADC input, based on the datasheet: DS13514 - Rev 2 specifically table 12, it appears it can be used as ADC_IN15, However in STM32Cube IDE , PA11 can not be ass...

AndFel_0-1743370150027.png AndFel_1-1743370433676.png
AndFel by Associate II
  • 1900 Views
  • 3 replies
  • 0 kudos

Resolved! How is SCLH and SCLL calculated in I2C_TIMINGR?

I have read the document RM0433 and AN4235, but the calculation is still a puzzle. For example, if my I2C frequency = 1MHz, I2C clock source frequency = 170MHz, AF=on, DF=off, rise time = 80ns, fail time = 10ns, how do you get the SCLH = 0x10 and SCL...

SHU.1 by Associate
  • 3537 Views
  • 2 replies
  • 0 kudos

NUCLEO-H723ZG BOARD ADC NOISE

Hi, I am planning on using STM32H723ZGT6 chip on one of my boards. I got the NUCLEO-H723ZG to measure the 12-bit ADC noise. From the datasheet for STM32H723ZGT6, the max ADC noise should be 5 times the LSB or 4.02mV. (1 LSB = 3.3/4096) I am getting 2...

josegalicia_0-1741886842223.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.