STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H747i-disco 10Mhz Uart Rx interrupt problem

Hello ST experts, i need help about using STM32H747i-discoI'm testing Uart Tx(DMA)-Rx(Interrupt). My goal is 10Mhz uart tx-rx.The problem is that i success 750khz, but fail to Rx when baudrate 1Mhz~10Mhz. I set the disco 480Mhz setting (hw SB setting...

soulshine by Associate II
  • 2600 Views
  • 7 replies
  • 2 kudos

Resolved! Programming STM32C011J6M6 with Arduino IDE

Hello, I'm using an STM32C011J6M6 with the Arduino IDE to register with theST25DV64KC-IE6S3 's EEPROM. I previously used the ATTiny85 and would like to replace it with the STM32C0 to maintain the entire solution with ST components. I made some change...

ThreadX conflict with Timer1

Hi,I'm using TIM1 in Encoder mode while running ThreadX in the program in STM32H523. I encountered an issue where TIM1→CNT only toggles between 0 and 1 when rotating the encoder. However, when I deactivated ThreadX, the encoder worked fine. I haven't...

Jeff4 by Associate II
  • 1769 Views
  • 5 replies
  • 0 kudos

How to calculate i2c timingR for stm32H5

I need help understanding how to calculate I2C timingR without using stm32cubemx.I have searched high and low and I haven't had any luck finding solutions.I want to create function that helps me manually setup the timing with different inputs without...

A_Bit_More_1-1743700131984.png A_Bit_More_2-1743700187180.png

custom board using STM32G431 and TCPP03

Hi @Susu , I have designed a custom board using STM32G431 and TCPP03, am able to see the debug traces in CubeMonUCPD. But unable to get the GUI interface and board is not detected. I have enabled the GUI interface in cubemx ,still not working.Can you...

RJain.1 by Associate III
  • 2544 Views
  • 5 replies
  • 1 kudos

How to determine proper DSI, LTDC and HDMI timings?

This is my first time working with any DSI/LTDC/HDMI related stuff, so I'm still figuring a lot of this stuff out and could use some help figuring out how times and clock speeds all interact. I'm using the STM32H757 Eval board.  I have it working wit...

JKaz.1 by Associate III
  • 4815 Views
  • 8 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.