cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F413xx + MCP2517FD CANFD Controller

Rajitha_at_UoM
Associate II

Can I do CANFD communication using external CAN controllers(ex:MCP2517FD)?
This MCP2517FD controller works with SPI.

Microcontroller I'm using: STM32F413VGT3

1 ACCEPTED SOLUTION

Accepted Solutions
mƎALLEm
ST Employee

Hello,

MCP2517FD is just an a SPI/CAN converter so it can be used with any MCU having SPI interface including STM32 MCU.

Hope that answers your question.

PS: but if your question: "Can I do CANFD communication using MCP2517FD?" the answer is yes:

mALLEm_0-1743593872823.png

And you need to contact Microchip on their forums for more details.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3
mƎALLEm
ST Employee

Hello,

MCP2517FD is just an a SPI/CAN converter so it can be used with any MCU having SPI interface including STM32 MCU.

Hope that answers your question.

PS: but if your question: "Can I do CANFD communication using MCP2517FD?" the answer is yes:

mALLEm_0-1743593872823.png

And you need to contact Microchip on their forums for more details.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

Thank you very much.

Thank you very much.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.